ota_mcuboot_server_wifi
Overview
This application demonstrates OTA update through HTTP server based on lwIP TCP/IP stack with FreeRTOS. The user uses an Internet browser to upload new version of firmware and restarts the board to perform the update
Supported Boards
Prepare the Demo
The demo requires MCUBoot bootloader to be present in the FLASH memory to function properly. It is recommended to build and program the bootloader first, then go on with the application. Please refer to respective readme of the mcuboot_opensource example and follow the steps there before you continue.
Before building the example application select Wi-Fi module macro in the
app_config.h
. (see#define WIFI_<SoC Name>BOARD<Module Name>
). For more information about Wi-Fi module connection see coresponding readme in WiFi examples directory.Prior launching the demo it is recommended to pre-build image with modified version of the application to test the OTA update process.
Connect a USB cable between the PC host and the OpenSDA(or USB to Serial) USB port on the target board.
Open a serial terminal on PC for OpenSDA serial(or USB to Serial) device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Unix line ending using
\n
Install WiFi connectivity module into SD or M.2 slot.
Running the demo
To get the application properly executed by the bootloader, it is necessary to put signed application image to the primary application partition. There are multiple options how to achieve that, however in principle the are two main methods (both presuming the bootlaoder is already in place):
programing signed application image to the primary application partition using an external tool (direct method)
jump-starting the application by debugger, performing OTA update with the signed image, resetting the board and letting the bootloader to perform update (indirect method)
The latter method is described step by step below:
Load the demo project and build it. Known issue: MDK linker issues warning about unused boot_hdr sections. This does not affect the functionality of the example.
Prepare signed image of the application from raw binary as described in the mcuboot_opensource readme.
In case of MCUXpress raw binary may not be generated automatically. Use binary tools after right clicking Binaries/.axf file in the project tree to generate it manually.
Launch the debugger in your IDE to jump-start the application.
In case of MCUXpresso IDE the execution stalls in an endless loop in the bootloader. Pause the debugging and use debugger console and issue command
jump ResetISR
.
When the demo runs successfully, the terminal will display the following:
Initializing WiFi connection... MAC Address: D8:C0:A6:C0:B0:57 [net] Initialized TCP/IP networking stack WLAN initialized WLAN FW Version: w8978o-V0, RF878X, FP91, 16.91.10.p185, WPA2_CVE_FIX 1, PVE_FIX 1 Successfully initialized WiFi module Starting Access Point: SSID: nxp-ota, Chnl: 1 [wlcm] Warn: NOTE: uAP will automatically switch to the channel that station is on. Soft AP started successfully This also starts DHCP Server with IP 192.168.1.1 Join 'nxp-ota' network and visit http://192.168.1.1
Connect you PC to WiFi network provided by the board (SSID: nxp-ota, password: NXP0123456789). Your PC should acquire IP configuration automatically via DHCP.
Open web browser and type
http://192.168.1.1
(IP address of the board) on the browser address bar. The browser should show the main web page of the example. Note: Be sure to include http protocol specifier in the address bar, so that your browser attempts to establish HTTP connection using port 80Go to OTA page, select file with udpated firmware and upload it.
After the file is uploaded, click Reboot button to start newly uploaded firmware in test mode.
Once the updated firmware executes, the accept button becomes active. Click it to make the update permanent. Note: Make sure your computer is connected to the AP provided by the board at this point as it might automatically connect to another AP during the reboot.
Known issue: Browser may not display progress of the upload. This is an issue of the browser rather than OTA demo. It is possible to watch upload progress in the attached serial console.
Modifying content of static web pages
To modify content available through the web server you must complete following steps:
Modify, add or delete files in folder
boards\<board_name>\lwip_examples\lwip_httpsrv_ota\webpage
.Run the script file
middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl <directory name>
to generate newhttpsrv_fs_data.c
. Make sure to execute it from a folder where the filehttpsrv_fs_data.c
is. For example:C:\sdk\boards\<board_name>\lwip_examples\lwip_httpssrv_ota> C:\sdk\middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl webpage Processing file webpage/favicon.ico Processing file webpage/httpsrv.css Processing file webpage/index.html Processing file webpage/NXP_logo.png Processing file webpage/ota.shtml Processing file webpage/ota_reboot.html Processing file webpage/request.js Processing file webpage/welcome.html Done.
Make sure the
httpsrv_fs_data.c
file has been overwritten with the newly generated content.Re-compile the HTTP server application example and download it to your board.