soem_gpio_pulse_netc_freertos
Overview
This example demonstrates how to use the Simple Open EtherCAT Master (SOEM) Library to communicate with EhterCAT devices.
In this example there are three EhterCAT devices, one EtherCAT Coupler EK1100, one EtherCAT Terminal EL2008 (slave0), and one EtherCAT Terminal EL1018 (slave1).
This example controls a stepper motor system using two outputs and one input remote IO: Outputs: -Pluse: The pulse signal with the period of 200us and the duty cycle of 50%. -Dir: The direction signal. Inputs: -Limit signal: This signal comes from the Limit Switchs on the stepper motor system. The Dir signal changes once when one of the Limit Switchs has been touched.
Running the demo
If the test passes, the led2 of slave0 lights up at 50% brightness.
If the stepper motor system is not setup properly, you can get information from the console log and the led4 status of slave0.
When the demo is running, the serial port will output:
Start the soem_gpio_pulse FreeRTOS example…
ec_init on enet0 succeeded.
ec_config_init 0 3 slaves found and configured.
ec_config_map_group IOmap:80000089 group:0
Slave 1, configadr 1001, state 12 Slave 2, configadr 1002, state 12 Slave 3, configadr 1003, state 12 SII Isize:0 SII Osize:0 ISIZE:0 0 OSIZE:0 SM programming SII Isize:0 SII Osize:8 SM0 length 8 ISIZE:0 0 OSIZE:8 SM programming SM0 Type:3 StartAddr: f00 Flags: 90044 SII Isize:8 SM0 length 8 SII Osize:0 ISIZE:8 8 OSIZE:0 SM programming SM0 Type:4 StartAddr:1000 Flags: 10000 OUTPUT MAPPING FMMU 0 SM0 slave 2 Outputs 80000089 startbit 0 =Slave 3, INPUT MAPPING FMMU 0 SM0 Inputs 8000008A startbit 0 IOmapSize 2 Slaves mapped, state to SAFE_OP.
oloop = 1, iloop = 1
segments : 1 : 2 0 0 0
Request operational state for all slaves
Calculated workcounter 3
Operational state reached for all slaves.