soem_servo_motor_bm

Overview

This example demonstrates how to use the Simple Open EtherCAT Master (SOEM) Library to control servo-motor.

In this example there are 2 servo-motor: DELTA_ASDA_B3 * 1 INOVANCE_SV680 * 1

Running the demo

If the test passes, D6 LED light will light up and the motor will start to retate.

When the demo is running, the serial port will output:

NETC EP frame loopback example start. Starting motion task ec_init on netc0 succeeded. ec_config_init 0 Copy SII slave 2 from 1. Copy SII slave 3 from 1. … 31 slaves found and configured. ec_config_map_group IOmap:20000664 group:0

Slave 1, configadr 1001, state 2 CoE Osize:56 Isize:88 … SM programming SM2 Type:3 StartAddr:1200 Flags: 10064 … IOmapSize 558 Slaves mapped, state to SAFE_OP. segments : 1 : 558 0 0 0 Request operational state for all slaves Calculated workcounter 93 Request operational state for all slaves Calculated workcounter 93 Operational state reached for all slaves.

User can connect the oscilloscope to R35 register to observe processing time and jitter. By raising the pin of the LED light before sending the Ethercat packet and lowering the pin of the LED light after sending the Ethercat packet. Measure the interval time using an oscilloscope to evaluate SOEM performance. Note: Detailed SOEM performance please refter to EtherCAT Benchamrk.

Supported Boards