Maestro on Zephyr
Based on and tested with Zephyr version, given by tag v4.0.0
Tested with Zephyr SDK version 16.4
To see the pre-built documentation, see: README.html. Also see the documentation section.
Maestro environment setup
Follow these steps to set up a Maestro development environment on your machine.
If you haven’t already, please follow this guide to set up a Zephyr development environment and its dependencies first:
Cmake
Python
Devicetree compiler
West
Zephyr SDK bundle
Get Maestro. You can pick either of the options listed below. If you need help deciding which option is the best fit for your needs, please see the FAQ.
Freestanding Maestro - This option pulls in only Maestro’s necessary dependencies.
Run:
1. west init -m <maestro repository url> --mr <revision> --mf west-freestanding.yml <foldername> 2. cd <foldername> 3. west update
Maestro as a Zephyr module
To include Maestro into Zephyr, update Zephyr’s
west.yml
file:projects: name: maestro url: <maestro repository url> revision: <revision with Zephyr support> path: modules/audio/maestro import: west.yml
Then run
west update maestro
command.
Build and run Maestro example
These steps will guide you through building and running Maestro samples.
You can use either the command line utilizing Zephyr’s powerful west
tool or you can use VS Code’s GUI.
Detailed steps for both options are listed below.
Using command line
See Zephyr’s Building, Flashing and Debugging guide if you aren’t familiar with it yet.
To build a project, run:
west build -b <board> -d <output build directory> <path to example> -p
For example, this compiles VIT example for rd_rw612_bga board:
1. cd maestro/zephyr 2. west build -b rd_rw612_bga -d build samples/vit -p
To run a project, run:
west flash -d <directory>
e.g.:
west flash -d build
To debug a project, run:
west debug -d <directory>
e.g.:
west debug -d build
Using MCUXpresso for VS Code
For this you have to have NXP’s MCUXpresso for VS Code extension installed.
Import your topdir as a repository to MCUXPresso for VS Code:
Open the MCUXpresso Extension. In the Quickstart Panel click Import Repository.
In the displayed menu click LOCAL tab and select the folder location of your topdir.
Click Import.
The repository is successfully added to the Installed Repositories view once the import is successful.
To import any project from the imported repository:
In the Quickstart Panel click Import Example from Repository.
For Repository select your imported repository.
For Zephyr SDK the installed Zephyr SDK is selected automatically. If not, select one.
For Board select your board (make sure you’ve selected the correct revision).
For Template select the folder path to your project.
Click the Create button.
Build the project by clicking the Build Selected icon (displayed on hover) in the extension’s Projects view. After the build, the debug console window displays the memory usage (or compiler errors if any).
Debug the project by clicking the Debug (play) icon (displayed on hover) in the extension’s Projects view.
The execution will pause. To continue execution click Continue on the debug options.
In the SERIAL MONITOR tab of your console panel, the application prints the Zephyr boot banner during startup and then prints the test results.
Folder structure
maestro/
├─── ...
└─── zephyr/ All Zephyr related files
├── samples/ Sample examples
├── tests/ Tests
├── audioTracks/ Audio tracks for testing
├── doc/ Documentation configuration for Sphinx
├── wrappers/ NXP SDK Wrappers
├── scripts/ Helper scripts, mostly for testing
├── module.yml Defines module name, Cmake and Kconfig locations
├── CMakeList.txt Defines module's build process
├── Kconfig Defines module's configuration
├── osa/ Deprecated. OSA port for Zephyr
└── ...
Supported elements and libraries
Here is the list of all features currently supported in Maestro on Zephyr. Our goal is to support all features in Maestro on Zephyr that are already supported in Maestro on NXP’s SDK and to extend them further.
Supported elements:
Memory source
Memory sink
Audio source
Audio sink
Process sink
Decoder
Encoder
Supported decoders:
WAV
MP3
FLAC
OPUS OGG
AAC
Supported encoders:
OPUS RAW
Supported libraries:
Examples support
All included examples use UART as output.
Examples are located in zephyr/tests
and zephyr/samples
directories.
List of included examples:
Examples support for specific boards:
Example |
RDRW612BGA |
LPCxpresso55s69 |
MIMXRT1060EVKB |
MIMXRT1170EVKB |
---|---|---|---|---|
YES |
TO BE TESTED |
TO BE TESTED |
TO BE TESTED |
|
YES |
TO BE TESTED |
TO BE TESTED |
TO BE TESTED |
|
In progress: OPUS RAW |
TO BE TESTED |
TO BE TESTED |
TO BE TESTED |
|
YES - WAV, FLAC, OPUS OGG |
TO BE TESTED |
TO BE TESTED |
TO BE TESTED |
|
YES |
TO BE TESTED |
TO BE TESTED |
TO BE TESTED |
Creating your own example
There are two ways to create your own example - you can either one of the included examples as a reference or you can create your own example from scratch by hand.
When creating your own example from scratch, set CONFIG_MAESTRO_AUDIO_FRAMEWORK=y
in your prj.conf
file. Then you can start enabling specific elements by setting CONFIG_MAESTRO_ELEMENT_<NAME>_ENABLE=y
.
However, the recommended way to edit config options is to open gui-config (or menuconfig) by calling west build -t guiconfig
.
Then you can use the graphical interface to interactively turn on/off the features you need.
Documentation
Please note, Maestro documentation is under reconstruction. It is currently mixing several tools and formats.
To see the pre-generated Maestro Zephyr documentation, see zephyr/doc/doc/README.html
To generate the Zephyr documentation, go under zephyr/doc
folder and execute make html
. Sphinx version sphinx-build 8.1.3
must be installed. Open doc/doc/html/README.hml
afterwards.
To see Maestro core documentation, go to the Maestro top directory and see README.md
.
FAQ
Should I choose the freestanding version of Maestro or should integrate it into my west instead?
Freestanding version of Maestro pulls in all the dependencies it needs including Zephyr itself.
Integrating it as a module is easier if you already have your Zephyr environment set up.