AP-STA mode {#topic_f7231db1-b1df-4e20-822f-02c97f3c11e8}

Features

Sub features

88W8987

IW416

IW611/IW612

RW610/RW612

AW611

88W8801

Simultaneous AP-STA operation (same channel)

AP-STA functionality

Y

Y

Y

Y

Y

Y

SAD

Software antenna diversity

Y

Y

Y

Y

Y

Y

Generic

Firmware download (parallel)[^1]

Y

Y

Y

N

Y

N

Generic

Secure boot

N

N

Y

Y

Y

N

Generic

Slim feature

N

Y

N

Y

N

N

Parent topic:Wi-Fi radio

[^1] Feature not enabled by default in the SDK. Refer to Feature enable and memory impact for the macro to enable the feature and the impact on the memory when enabling the feature.