Firmware version: From 16.91.21.p64.1 to 16.91.21.p82 {#topic_8a27a819-9318-4342-8300-d4e5059b23a6}

Component

Description

Wi-Fi

  • WPA3-R3 enabled APUT beacons does not have RSNXE when configured in H2E mode
  • Associated event is received even when connecting using wrong password
  • WFA APUT Low iperf TCP/UDP Tx throughput with Realtek station

Parent topic:Bug fixes and/or feature enhancements