NVM : Non-volatile memory module
Overview
In a standard Harvard-architecture-based MCU, the flash memory is used to store the program code and program constant data. Modern processors have a built-in flash memory controller that can be used under user program execution to store non-volatile data. The flash memories have individually erasable segments (sectors) and each segment has a limited number of erase cycles. If the same segments are used to store various kinds of data all the time, those segments quickly become unreliable. Therefore, a wear-leveling mechanism is necessary to prolong the service life of the memory. The NVM module in the connectivity framework provides a file system with a wear-leveling mechanism, described in the subsequent sections. The NvIdle() function handles the program and erase memory operations. Before resetting the MCU, NvShutdown() must be called to ensure that all save operations have been processed.
NVM boundaries and linker script requirement
Most of the MCUs have only a standard flash memory that the non-volatile (NV) storage system uses. The amount of memory that the NV system uses for permanent storage and its boundaries are defined in the linker configuration file though the following linker symbols :
NV_STORAGE_START_ADDRESS
NV_STORAGE_END_ADDRESS
NV_STORAGE_MAX_SECTORS
NV_STORAGE_SECTOR_SIZE
The reserved memory consists of two virtual pages. The virtual pages are equally sized and each page is using one or more physical flash sectors. Therefore, the smallest configuration is using two physical sectors, one sector per virtual page.
NVM Table
The Flash Management and Non-Volatile Storage Module holds a pointer to a RAM table. The upper layers of this table register information about data that the storage system should save and restore. An example of NVM table entry list is given below.
NVM Table entry
As show above, A NVM table entry contains a generic pointer to a contiguous RAM data structure, the number of elements the structure contains, the size of a single element, a table entry ID, and an entry type.
A RAM table entry has the following structure:
pData (4 bytes) is a pointer to the RAM memory location where the dataset elements are stored.
elemCnt (2 bytes) represents how many elements the dataset has.
elemSz (2 bytes) is the size of a single element.
entryID is a 16-bit unique ID of the dataset.
dataEntryType is a 16-bit value representing the type of entry (mirrored/unmirrored/unmirrored auto restore).
For mirrored datasets, pData must point directly to the RAM data. For unmirrored datasets, it must be a double pointer to a vector of pointers. Each pointer in this table points to a RAM/FLASH area. Mirrored datasets require the data to be permanently kept in RAM, while unmirrored datasets have dataset entries either in flash or in RAM. If the unmirrored entries must be restored at the initialization, NotMirroredInRamAutoRestore should be used. The entryID gUnmirroredFeatureSet_d should be set to 1 for enabling unmirrored entries in the application. The last entry in the RAM table must have the entryID set to gNvEndOfTableId_c.
The figure below provides an example of table entry :
When the data pointed to by the table entry pointer (pData) has changed (entirely or just a single element), the upper layers call the appropriate API function that requests the storage system to save the modified data. All the save operations (except for the synchronous save and atomic save) and the page erase and page copy operations are performed on system idle task. The application must create a task that calls NvIdle in an infinite loop. It should be created with OSA_PRIORITY_IDLE. However, the application may choose another priority. The save operations are done in one virtual page, which is the active page. After a save operation is performed on an unmirrored dataset, pData points to a flash location and the RAM pointer is freed. As a result, the effective data should always be allocated using the memory management module.
Active page
The active page contains information about the records and the records. The storage system can save individual elements of a table entry or the entire table entry. Unmirrored datasets can only have individual saves. On mirrored datasets, the save/restore functions must receive the pointer to RAM data. For example, if the application must save the third element in the above vector, it should send 0x1FFF8000 + 2 * elemSz. For unmirrored datasets, the application must send the pointer that points to the area where the data is located. For example, if the application must save the third element in the above vector, it should send 0x1FFF8000 + 2 * sizeof(void*).
The page validity is guaranteed by the page counter. The page counter is a 32-bit value and is written at the beginning and at the end of the active page. The values need to be equal to consider the page a valid one. The value of the page counter is incremented after each page copy operation. A page erase operation is performed when the system is formatted. It is also performed when the page is full and a new record cannot be written into that page. Before being erased, the full page is first copied (only the most recent saves) and erased afterward.
The validity of the Meta Information Tag (MIT), and, therefore, of a record, is guaranteed by the MIT start and stop validation bytes. These two bytes must be equal to consider the record referred by the MIT valid. Furthermore, the value of these bytes indicates the type of the record, whether it is a single element or an entire table entry. The nonvolatile storage system allows dynamic changes of the table within the RAM memory, as follows:
Remove table entry
Register table entry
A new table entry can be successfully registered if there is at least one entry previously removed or if the NV table contains uninitialized table entries, declared explicitly to register new table entries at run time. A new table entry can also replace an existing one if the register table entry is called with an overwrite set to true. This functionality is disabled by default and must be enabled by the application by setting gNvUseExtendedFeatureSet_d to 1.
The layout of an active page is shown below:
As shown above, the table stored in the RAM memory is copied into the flash active page, just after the table version. The “table start” and “table end” are marked by the table markers. The data pointers from RAM are not copied. A flash copy of a RAM table entry has the following structure:
Where:
entryID is the ID of the table entry
entryType represents the type of the entry (mirrored/unmirrored/unmirrored auto restore)
elemCnt is the elements count of that entry
elemSz is the size of a single element
This copy of the RAM table in flash is used to determine whether the RAM table has changed. The table marker has a value of 0x4254 (“TB” if read as ASCII codes) and marks the beginning and end of the NV table copy.
After the end of the RAM table copy, the Meta Information Tags (MITs) follow. Each MIT is used to store information related to one record. An MIT has the following structure:
Where:
VSB is the validation start byte.
entryID is the ID of the NV table entry.
elemIdx is the element index.
recordOffset is the offset of the record related to the start address of the virtual page.
VEB is the validation end byte.
A valid MIT has a VSB equal to a VEB. If the MIT refers to a single-element record type, VSB=VEB=0xAA. If the MIT refers to a full table entry record type (all elements from a table entry), VSB=VEB=0x55. Because the records are written to the flash page, the available page space decreases. As a result, the page becomes full and a new record does not have enough free space to be copied into that page.
In the example given below, the virtual page 1 is considered to be full if a new save request is pending and the page free space is not sufficient to copy the new record and the additional MIT. In this case, the latest saved datasets (table entries) are copied to virtual page 2.
In this example, there are five datasets (one color for each dataset) with both ‘full’ and ‘single’ record types.
R1 is a ‘full’ record type (contains all the NV table entry elements), whereas R3, R4, R6 and R11 are ‘single’ record types.
R2 – full record type; R15 – single record type
R5, R13 – full record type; R10, R12 – single record type
R8 – full record type
R7, R9, R14, R16 – full record type
As shown above, the R3, R4, R6, and R11 are ‘single’ record types, while R1 is a ‘full’ record type of the same dataset. When copied to virtual page 2, a defragmentation process takes place. As a result, the record copied to virtual page 2 has as much elements as R1, but individual elements are taken from R3, R4, R6, and R11. After the copy process completes, the virtual page 2 has five ‘full’ record types, one for each dataset. |This is illustrated below:
Finally, the virtual page 2 is validated by writing the PC value and a request to erase virtual page 1 is performed. The page is erased on an idle task, sector by sector where only one sector is erased at a time when idle task is executed.
If there is any difference between the RAM and flash tables, the application must call RecoverNvEntry for each entry that is different from its RAM copy to recover the entry data (ID, Type, ElemSz, ElemCnt) from flash before calling NvInit. The application must allocate the pData and change the RAM entry. It can choose to ignore the flash entry if the entry is not desired. If any entry from RAM differs from its flash equivalent at initialization, a page copy is triggered that ignores the entries that are different. In other words, data stored in those entries is lost.
The application can check if the RAM table was updated. In other words, if the MCU program was changed and the RAM table was updated, using the function GetFlashTableVersion and compare the result with the constant gNvFlashTableVersion_c. If the versions are different, NvInit detects the update and automatically upgrades the flash table. The upgrade process triggers a page copy that moves the flash data from the active page to the other one. It keeps the entries that were not modified intact and it moves the entries that had their elements count changed as follows:
If the RAM element count is smaller than the flash element count, the upgrade only copies as many elements as are in RAM.
If the RAM element count is larger than the flash element count, the upgrade copies all data from flash and fills the remaining space with data from RAM. If the entry size is changed, the entry is not copied. Any entryIds that are present in flash and not present in RAM are also not copied. This functionality is not supported if gNvUseExtendedFeatureSet_d is not set to 1.
ECC Fault detection
The KW45/K32W1 internal flash is organized in 16 byte phrases and 8kB sectors (minimal erase unit). Its flash controller is synthesized so that it generates ECC information and an ECC generator / checker. During the programming of internal flash, errors may accidentally happen and cause ECC errors as a flash phrase is being written. These may happen due to multiple reasons:
programmatic errors such as overwriting an already programmed phrase (transitioning bits from 0b to 1b). These are evitable by performing a blank check verification over phrase to be programmed, at the expense of processing power.
occurrence of power drop or glitches during a programming operation.
excessive wear of flash sector. The flash controller is capable of correcting one single ECC error but raises a bud fault whenever reading a phrase containing more than one ECC fault. Once an ECC error has ‘infected’ a flash phrase, the fault will remain and raise again at each read operation over the same phrase including blank check and prefetch. It can only be rid of by erasing the whole flash sector that contained the faulty phrase. In order to recover from situations where an ECC fault has occurred a gNvSalvageFromEccFault_d option has been added, which forces gNvVerifyReadBackAfterProgram_d to be defined to TRUE. If defined, the gNvVerifyReadBackAfterProgram_d option of the NVM module, causes the program to read back the programmed area after every flash programming operation. The verification is performed in safe mode if gNvSalvageFromEccFault_d is also defined. This is so as to detect ECC faults as early as possible as they appear, indeed when verifying a programming operation, one cannot be certain of the absence of ECC fault and avoid the bus fault. The safe API is thence used to perform the read back operation is performed using this safe API, so that we can tread in the flash and detect potential errors. The defects are detected on the fly whereas in the absence of safe read back, the error would cause a fault, potentially much later. During normal operation, assuming that no chip reset was provoked, this will consist in a single ECC fault either in the last record data or its meta information. Detecting such a fault calls for an immediate page copy to the other virtual page, so that the currently active page gets erased and the error gets cleared. Should the ECC fault occurs in the middle of a page copy operation, the switch of active page is postponed so that the fault page can be erased again and the copy can be restarted.
If the system underwent a power drop during a flash programming operation, sufficient to provoke a reset, at the ensuing reboot, ECC fault(s) may be present in the NVM area at the location that was being written. The detection is performed by an NVM sweeping mechanism, using the safe read API. That marks the faulty virtual page so that all subsequent reads within this virtual page are done with the safe API. If this case arises, a copy of the valid contents of the faulty page is attempted to the other virtual page. At NVM initialization, faults should be detected, either at the top of the meta data or at the bottom of the record area within the previous active page. This should guarantee that only the latest record write operation may be impaired. When the page copy has taken place, the faulty page is erased and the execution may resume. During NvCopyPage, when ‘garbage collecting’ occurs or whenever the current virtual active page needs to be transferred to the other virtual page, ECC errors are intercepted so that the operation can be attempted again in case of error. In case of NVM contents clobbering by programming errors, the salvage operation does its best to rescue as many records as possible but data will inevitably be lost.
An additional option -namely gInterceptEccBusFaults_d - was introduced in order to catch and correct ECC faults at Bus Fault handler level. Indeed, should an ECC bus fault fire, in spite of the precautions taken with NVM’s gNvSalvageFromEccFault_d, we verify if the fault belongs to the NV storage. If so, a drastic policy can be adopted consisting in an erasure of the faulty sector. The corresponding Bus Fault handling is not part of the NVM, but dwells in the framework platform specific sources. Alternative handling could be implemented by the customer.
Save policy:
Execution of program and erase operations on a flash an MCU core fetches code from cause perturbations of the core activity or requires to place critical code in RAM so that real-time ISR can still be served. The penalty of a sector erase is much higher than a simple program operation. The NVM is designed so as to limit the erase operations at ‘garbage collecting’ time, so that flash wear is limited and no time is wasted. Several write policies are implemented to cope with the application constraints, one synchronous mode API and several posted write APIs. Among the posted write policies, the gNvmSaveOnIdleTimerPolicy_d compilation option selects a mode where flash write operations occur at time interval within the Idle task. Another option exists to ‘randomize’ the time interval with some jitter.
NvSyncSave performs a write synchronously with the disadvantage of stalling processor activity until comp
NvSaveOnCount posts a pending write operation and postpones the actual flash operation until number of record updates has reached a maximum. The actual write happens during Idle Task execution.see NvSetCountsBetweenSaves related API.
NvSaveOnInterval: posts a pending write operation and postpones the actual flash operation until the predefined number of ticks has elapsed. Optional mode - Active if (gNvmSaveOnIdleTimerPolicy_d & gNvmUseSaveOnTimerOn_c). see NvSetMinimumTicksBetweenSaves related API. Note that gNvmUseSaveIntervalJitter_c policy is a sub-option of gNvmSaveOnIdleTimerPolicy_d used to randomize slightly the time at which the write operation will happen.
Constant macro definition
gNvStorageIncluded_d : If set to TRUE, it enables the whole functionality of the nonvolatile storage system. By default, it is set to FALSE (no code or data is generated for this module).
gNvUseFlexNVM_d : If set to TRUE, it enables the FlexNVM functionality of the nonvolatile storage system. By default, it is set to FALSE. If FlexNVM is used, the standard nonvolatile storage system is disabled.
gNvFragmentation_Enabled_d : Macro used to enable/disable the fragmented saves/restores (a particular element from a table entry can be saved or restored). It is set to FALSE by default.
gNvUseExtendedFeatureSet_d : Macro used to enable/disable the extended feature set of the module:
Remove existing NV table entries
Register new NV table entries
Table upgrade
It is set to FALSE by default.
gUnmirroredFeatureSet_d : Macro used to enable unmirrored datasets. It is set to 0 by default.
gNvTableEntriesCountMax_c : This constant defines the maximum count of the table entries (datasets) that the application is going to use. It is set to 32 by default.
gNvRecordsCopiedBufferSize_c : This constant defines the size of the buffer used by the page copy function, when the copy operation performs defragmentation. The chosen value must be bigger than the maximum number of elements stored in any of the table entries. It is set by default to 64.
gNvCacheBufferSize_c : This constant defines the size of the cache buffer used by the page copy function, when the copy operation does not perform defragmentation. The chosen value must be a multiple of 8. It is set by default to 64.
gNvMinimumTicksBetweenSaves_c : This constant defines the minimum timer ticks between dataset saves (in seconds). It is set to 4 by default.
gNvCountsBetweenSaves_c : This constant defines the number of calls to ‘NvSaveOnCount’ between dataset saves. It is set to 256 by default.
gNvInvalidDataEntry_c : Macro used to mark a table entry as invalid in the NV table. The default value is 0xFFFFU.
gNvFormatRetryCount_c : Macro used to define the maximum retries count value for the format operation. It is set to 3 by default.
gNvPendingSavesQueueSize_c : Macro used to define the size of the pending saves queue. It is set to 32 by default.
gFifoOverwriteEnabled_c : Macro used to enable overwriting older entries in the pending saves queue (if it is full). If it is FALSE and the queue is full, the module tries to process the oldest save in the queue to free a position. It is set to FALSE by default.
gNvMinimumFreeBytesCountStart_c : Macro used to define the minimum free space at initialization. If the free space is smaller than this value, a page copy is triggered. It is set by default to 128.
gNvEndOfTableId_c : Macro used to define the ID of the end-of-table entry. It is set to 0xFFFEU by default. No valid entry should use this ID.
gNvTableMarker_c : Macro used to define the table marker value. The table marker is used to indicate the start and the end of the flash copy of the NV table. It is set to 0x4254U by default.
gNvFlashTableVersion_c : Macro used to define the flash table version. It is used to determine if the NVM table was updated. It is set to 1 by default. The application should modify this every time the NVM table is updated and the data from NVM is still required.
gNvTableKeptInRam_d : Set gNvTableKeptInRam_d to FALSE, if the NVM table is stored in FLASH memory (default). If the NVM table is stored in RAM memory, set the macro to TRUE.
gNvVerifyReadBackAfterProgram_d : set by default force verification of NVM programming operations. Is forced implicitly when gNvSalvageFromEccFault_d is defined.
gNvSalvageFromEccFault_d : use safe flash API to read from flash, and provide corrective action when ECC fault is met.