Known issues

Known issues listed on this page and tagged with the latest official release version are valid for the current state of development. Use the drop-down filter to see known issues for previous releases and check if they are still valid.

A known issue can list one or both of the following entries:

  • Workaround:

    Some known issues have a workaround. Sometimes, they are discovered later and added over time.

Examples

LPSPI b2b examples transfer fail on iar/armgcc flash target.

Due to the latency of instruction retrieval (XiP), LPSPI-related flash target examples may fail. The failure happens because the data is not retrieved in time from FIFO on the receiving end.

Affected platforms: evkmcimx7ulp

Workaround: To prevent the failure and boost the instruction fetch performance, place the fsl_lpspi.c file in the SRAM. Apply the patch as below,

$ git diff  MCIMX7U5xxxxx_cm4_flash.ld
diff --git a/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld b/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld
index b29b41a2b1..91dc0782e5 100644
--- a/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld
+++ b/MCIMX7U5/gcc/MCIMX7U5xxxxx_cm4_flash.ld
@@ -68,10 +68,22 @@ SECTIONS
.text :
{
    . = ALIGN(4);
-    *(.text)                 /* .text sections (code) */
-    *(.text*)                /* .text* sections (code) */
-    *(.rodata)               /* .rodata sections (constants, strings, etc.) */
-    *(.rodata*)              /* .rodata* sections (constants, strings, etc.) */
+    *(EXCLUDE_FILE(
+        /* Exclude flash and frequently executed functions from XIP */
+        */fsl_lpspi.c.obj
+    ) .text)                 /* .text sections (code) */
+    *(EXCLUDE_FILE(
+        /* Exclude flash and frequently executed functions from XIP */
+        */fsl_lpspi.c.obj
+    ) .text*)                /* .text* sections (code) */
+    *(EXCLUDE_FILE(
+        /* Exclude flash and frequently executed functions from XIP */
+        */fsl_lpspi.c.obj
+    ) .rodata)               /* .rodata sections (constants, strings, etc.) */
+    *(EXCLUDE_FILE(
+        /* Exclude flash and frequently executed functions from XIP */
+        */fsl_lpspi.c.obj
+    ) .rodata*)              /* .rodata* sections (constants, strings, etc.) */
    *(.glue_7)               /* glue arm to thumb code */
    *(.glue_7t)              /* glue thumb to arm code */
    *(.eh_frame)
@@ -173,6 +185,7 @@ SECTIONS
    __quickaccess_start__ = .;
    . = ALIGN(32);
    *(CodeQuickAccess)
+    /* Explicit placement of flash and frequently executed functions in SRAM  */
+    */fsl_lpspi.c.obj(.text .text* .rodata .rodata*)
    *(DataQuickAccess)
    . = ALIGN(128);
    __quickaccess_end__ = .;
Maximum file path length in Windows 7 operating system

The Windows 7 operating system imposes a 260-character maximum length for file paths. When installing the MCUXpresso SDK, place it in a directory close to the root to prevent file paths from exceeding the maximum character length specified by the Windows operating system. The recommended location is the C:\<folder>.

Affected platforms: evkbimxrt1050 evkbmimxrt1060 evkbmimxrt1170 evkcmimxrt1060 evkmcimx7ulp evkmimx8mm evkmimx8mn evkmimx8mnddr3l evkmimx8mp evkmimx8mq evkmimxrt1010 evkmimxrt1015 evkmimxrt1020 evkmimxrt1024 evkmimxrt1040 evkmimxrt1060 evkmimxrt1064 evkmimxrt1160 evkmimxrt1170 evkmimxrt1180 evkmimxrt595 evkmimxrt685 frdmk22f frdmk32l2a4s frdmk32l2b frdmk32l3a6 frdmke02z40m frdmke15z frdmke16z frdmke17z frdmke17z512 frdmmcxa153 frdmmcxa156 frdmmcxc041 frdmmcxc242 frdmmcxc444 frdmmcxn236 frdmmcxn947 frdmmcxw71 k32w148evk kw45b41zevk kw45b41zloc lpc845breakout lpcxpresso51u68 lpcxpresso54628 lpcxpresso54s018 lpcxpresso54s018m lpcxpresso55s06 lpcxpresso55s16 lpcxpresso55s28 lpcxpresso55s36 lpcxpresso55s69 lpcxpresso802 lpcxpresso804 lpcxpresso824max lpcxpresso845max lpcxpresso860max mc56f80000evk mc56f81000evk mc56f83000evk mcxn5xxevk mcxn9xxevk mimxrt685audevk rdrw612bga twrkm34z50mv3 twrkm34z75m twrkm35z75m twrmc56f8200 twrmc56f8400

New Project Wizard compile failure

The following components request the user to manually select other components that they depend upon in order to compile. These components depend on several other components and the New Project Wizard (NPW) is not able to decide which one is needed by the user.

Note: xxx means core variants, such as, cm0plus, cm33, cm4, cm33_nodsp.

**Components:**issdk_mag3110, issdk_host, systick, gpio_kinetis, gpio_lpc, issdk_mpl3115, sensor_fusion_agm01, sensor_fusion_agm01_lpc, issdk_mma845x, issdk_mma8491q, issdk_mma865x, issdk_mma9553, and CMSIS_RTOS2.CMSIS_RTOS2, and components which include cache driver, such as enet_qos.

Also for low-level adapter components, currently the different types of the same adapter cannot be selected at the same time.

For example, if there are two types of timer adapters, gpt_adapter and pit_adapter, only one can be selected as timer adapter

in one project at a time. Duplicate implementation of the function results in an error.

Note: Most of middleware components have complex dependencies and are not fully supported in new project wizard. Adding a middleware component may result in compile failure.

CMSIS PACK new project compile failure

The generated configuration cannot be applied globally. The components, serial_manager_usb_cdc_virtual and serial_manager_usb_cdc_virtual_xxx (xxx means core variants like cm0plus, cm33, cm4, and cm33_nodsp) are unsupported for new project wizard of CMSIS pack and will lead to compile failure if selected while creating new project(s).

Affected platforms: evkbmimxrt1160 evkbmimxrt1170

Low speed devices not supported

The host examples cannot support low-speed devices

Affected platforms:  mimxrt685audevk rdrw612bga

IAR cannot debug RAM application with J-Link

Currently, IAR will call J-Link reset after the application is downloaded to SRAM, but such operation will cause SRAM data lost.

Affected platforms: mimxrt685audevk rdrw612bga lpcxpresso54s018 lpcxpresso54s018m

RAM targets build issue in CMSIS bsp pack

CMSIS pack does not support different macro definitions for different targets, all RAM targets for projects inside CMSIS BSP PACKs for RT10XX boards will get the same macro definitions with Flash targets, resulting in build failure. To pass build for RAM targets, manually update the XIP_EXTERNAL_FLASH and XIP_BOOT_HEADER_ENABLE value to 0 in RTE_Components.h.

Affected platforms: evkmimxrt1015 evkmimxrt1020 evkmimxrt1024 evkmimxrt1060 evkmimxrt1064

Non XIP target debug issue on toolchain MDK

When debugging non XIP targets in flash boot mode, if application changes any settings which have impacts on flexspi, the build output window might show “Debug access failed” when start debugging next time. It is recommended to keep the board in serial downloader mode when debugging non XIP targets.

Affected platforms: evkmimxrt1010 evkmimxrt1015 evkmimxrt1020 evkmimxrt1024 evkmimxrt1060 evkmimxrt1064

MCUXpresso IDE limitation

Cannot debug cm4 sdram related demos with CMSIS-DAP. MCUXpresso IDE does not support initialization of sdram when debugging.

Affected platforms: evkbmimxrt1160 evkbmimxrt1170

IAR debug limitation

CM4 flash target demos cannot be debugged on IAR with JLINK.

Affected platforms: evkbmimxrt1160 evkbmimxrt1170

Extra option required when using CMSIS-DAP to debug

When using CMSIS-DAP to debug CM4 sdram related target in IAR, such as flexspi_nor_sdram and sdram_txt, an extra option must be specified in the debugger settings. For details, see [IAR debug limitation](iar_debug_limitation.md).

Affected platforms: evkbmimxrt1160 evkbmimxrt1170

Corrupted data in freertos_lpspi_b2b (slave) example

Corrupted data in freertos_lpspi_b2b(slave) example. Tool: Keil MDK Target: freertos_lpspi_b2b_slave_flexspi_nor_debug.

Affected platforms: evkbmimxrt1060 evkbmimxrt1064

Workaround: Changing the optimization level from -01 to -00 can avoid the issue. However, the optimization level -O1 is not the root cause

USBFS controller issue

Because of the USBFS controller design issues, the USB host suspend/resume demos (usb_suspend_resume_host_hid_mouse) of the full speed controller do not support the low speed device directly

Affected platforms: frdmk32l2a4s frdmmcxc041

FreeRTOS issue

When generating a new FreeRTOS project with New Project Wizard tool, the user should deassert the macro option “configUSE_PORT_OPTIMISED_TASK_SELECTION” in the “FreeRTOSConfig.h” file while it is not being used in the template project for some Cortex-M0+ devices or it may not pass the compiling.

Affected platforms: frdmk32l2b frdmmcxc242 frdmmcxc444

Workaround: Here is a workaround to avoid real reset, with the cost of no any reset during the debugging, and hardware status uncleared.

  1. Build and debug IAR project once and see the settings folder created.

  2. Create the _.JLinkScript file in the settings folder with the following contents.

    ` void ResetTarget(void) { JLINK_TARGET_Halt(); } `

  3. Debug the project again and now it can work.

    |![](images/jlink_issue.png “hello_world JLink script example”)


USB high-speed interrupt endpoint issue

If the user wants to use a high-speed interrupt endpoint, the maximum packet size should be 512 bytes.

Affected platforms: lpcxpresso54s018 lpcxpresso54s018m

Debug SRAM target with J-Link on MCUXpresso IDE issue

If using the J-Link to Debug SRAM target on the IDE, when clicking the Restart button, the debug fails. The issue is caused because the integrity of the SRAM image cannot be guaranteed after it has been executed, and the MCUXpresso IDE does not reload the code before restarting. Plain load images (images loaded from external SPI flash to SRAMX by the ROM bootloader then executed) cannot be debugged using MCUXpresso version 11.0.0. Code should be developed using the SRAM debug method, then programmed into flash once debugging is completed. For more information, see the Getting Started with MCUXpresso SDK User’s Guide (document MCUXSDKGSUG).

Affected platforms: lpcxpresso54s018

Cannot add SDK components into FreeRTOS projects

It is not possible to add any SDK components into FreeRTOS project using the MCUXpresso IDE New Project wizard.

Affected platforms: frdmke17z frdmke17z evkbimxrt1050 evkmcimx7ulp evkmimx8mm evkmimx8mn evkmimx8mp evkmimx8mq evkmimxrt1010 evkmimxrt1015 evkmimxrt1020 evkmimxrt1064 evkmimxrt595 evkmimxrt685 evkbmimxrt1060 evkcmimxrt1060 frdmk22f frdmk32l2a4s frdmk32l2b frdmk32l3a6 frdmke02z40m frdmke16z lpcxpresso54s018 lpc845breakout lpcxpresso54s018m lpcxpresso55s06 lpcxpresso55s28 lpcxpresso55s69 lpcxpresso802 lpcxpresso804 evkmimxrt1024 eevkbmimxrt1060 evkcmimxrt1060 evkmimxrt1160 evkbmimxrt1170 twrkm34z50mv3 twrkm34z75m frdmmcxc242 frdmk22f pcxpresso51u68 lpcxpresso54628

safety_iec60730b cloned project fails to build

When you use the MCUXpresso Config Tool to clone the “safety_iec60730b” project in MCUXpresso SDK package, the created project fails to build. The build fails because the post-build setup for CRC is incorrect. Therefore, It is recommended to use the “safety_iec60730b” project in MCUXpresso SDK package.

Affected platforms: evkbimxrt1050 v2024-12-00-pvw2 v2024-12-00 evkbimxrt1050 evkmimxrt1010 evkmimxrt1020 evkmimxrt1024 frdmk32l2a4s lpcxpresso55s28

Importing FTM_PDB_ADC16 project into MCUXpresso Config tool reports FTM driver error

When you import the FTM_PDB_ADC16 project using the MCUXpresso Config Tool an error is prompted. The error prompts that the FTM driver is not aligned with the peripheral components. It is recommended not to import this project into the MCUXpresso Config Tool.

Affected platforms: frdmk22f frdmke15z

Build warning in freertos_tickless example

A build warning appears in the freertos_tickless example while working in the ArmGCC environment. .. code-block:: none

c:cpkgcmsiscoreincludecore_cm0plus.h:854:52: warning: array subscript 14 is above array bounds of ‘volatile uint32_t[8]’ {aka ‘volatile long unsigned int[8]’} [-Warray-bounds].

Affected platforms: k32w148evk

Example freertos_lpspi fail before the console output

The example freertos_lpspi fails before the message “LPSPI master transfer completed successfully.” appears in the console output.

Console output:

``` FreeRTOS LPSPI example start. This example use one lpspi instance as master and another as slave on a single board. Master and slave are both use interrupt way. Please make sure you make the correct line connection. Basically, the connection is: LPSPI_master – LPSPI_slave

CLK – CLK PCS – PCS SOUT – SIN SIN – SOUT —

```

—

Affected platforms: frdmk32l2a4s frdmk32l2b frdmk32l3a6

Example freertos_spi fails in MCUXpresso IDE

The example freertos_spi fails in the MCUXpresso IDE environment.

Affected platforms: lpcxpresso54s018

Examples are not fully tested

The following examples are not fully tested in this Early Access Release. - wifi_setup - wifi_cert - wifi_test_mode - wifi_webconfig - wifi_ipv4_ipv6_echo - aws_shadow_wifi_nxp - aws_greengrass_discovery_wifi_nxp - aws_remote_control_wifi_nxp - aws_tests_wifi_nxp - lwip_httpssrv_ota_wifi - lwip_httpscli_ota_wifi - ota_demo_wifi

Affected platforms:

Some Azure examples cannot finish PHY Initializing on MCUXpresso

The following Azure examples cannot finish PHY initializing on MCUXpresso when running in Arm GCC, IAR, or Keil environment.

Examples: azure_amqp, azure_http, azure_mqtt, azure_amqp_rc, azure_http_rc, and azure_mqtt_rc.

Affected platforms:

lwip_httpssrv_ota_wifi example fails to accept the new image on EVKMIMXRT685

After uploading the new image over https, and rebooting the board the new image starts. However, reboot starts it is not possible to accept the update and make it permanent. This issue is specific to combination of EVKMIMXRT685 board and AW-NM191NF-uSD Wi-Fi module. Other configurations are not affected.

Affected platforms: mimxrt685audevk mimxrt700evk

Board may reset itself when running SD card related cases

Board may reset itself when running SD card related cases. However, the issue is not reproduced if more power supply is connected.

Affected platforms: mimxrt685audevk mimxrt700evk

usb_device_mtp example cannot boot on Keil MDK µVision

After reset, the usb_device_mtp and usb_device_mtp_lite examples cannot boot successfully when using Keil MDK µVision. Adding the –predefine=”-DXIP_BOOT_HEADER_ENABLE=1” into Options for target > Linker > Misc controls can fix this issue.

Affected platforms: rdrw612bga

Log output may be mixed in shell/hfp example

When multiple tasks print the log, the serial port terminal output has the probability to appear mixed.

Affected platforms: rdrw612bga frdmrw612 evkmimxrt1160 evkbmimxrt1170 evkbmimxrt1060 evkcmimxrt1060

LE encryption failure causes connection to fail

There can be a corner case when LE link encryption can fail. This occurs when device under test (DUT); RT Bluetooth controller here, while waiting for the response to LL_SLAVE_FEATURES_REQ, instead receives the LL_ENC_REQ response from a remote device. This causes deadlock scenario where DUT and remote devices are stuck waiting for response from peer.

Affected platforms: rdrw612bga frdmrw612 evkmimxrt1160 evkbmimxrt1170 evkbmimxrt1060 evkcmimxrt1060

Connection disconnects with 7.5 ms connection interval

When wireless example works as a peripheral, the central role with 7. 5 ms connection interval connects to the wireless example. However, when using the 6th/7th/8th central to connect the wireless example, all the previous connections with the previous centrals are disconnected. When wireless example works as central and the connection interval is 7.5 ms, the 4th peripheral is not scanned.

Affected platforms: rdrw612bga frdmrw612 evkmimxrt1160 evkbmimxrt1170 evkbmimxrt1060 evkcmimxrt1060

a2dp sink demo: Noise may occur when phone plays music with other operations

Noise may occur when phone plays music with other operations. For example: - Switches the WIFI network of the phone when playing music - Switches music when playing the online music

Affected platforms: rdrw612bga frdmrw612 evkmimxrt1160 evkbmimxrt1170 evkbmimxrt1060 evkcmimxrt1060

Volume is very loud from codec in the a2dp sink and hfp demos

After connecting to the phone and playing music or calling, the codec volume is very loud.

Affected platforms: rdrw612bga frdmrw612

Wireless EdgeFast_Bluetooth stack is not supported by any kits

Wireless EdgeFast_Bluetooth stack can be downloaded by EVK-MIMXRT1060-AGM01, EVK-MIMXRT1060-OM13790HOST and EVK-MIMXRT1060-OM13588 in [https://mcuxpresso.nxp.com/en/welcome](https://mcuxpresso.nxp.com/en/welcome). However, it is not supported in these kits.

Affected platforms: evkmimxrt1060

Affected platforms: evkmimxrt1060

Affected platforms: evkmimxrt1170

Affected platforms: evkmimxrt685

Affected platforms: evkmimxrt595

aws_httpscli_corehttp example for evkmimxrt1160 issue in MCUXpressoIDE release target

The aws_httpscli_corehttp example for evkmimxrt1160 does not work correctly in MCUXpressoIDE release target. Use the debug target only in this IDE.

Affected platforms: evkmimxrt1160

Insufficient heap in ota_demo examples

The ota_demo examples, especially ota_demo_wifi, may run out of heap in the out-of-the-box configuration.

Affected platforms: evkbmimxrt1170

Workaround: Therefore, increasing the heap size to 200 KB in FreeRTOSConfig.h is recommended.

To increase the heap size, change line 62:

` #define configTOTAL_HEAP_SIZE ( ( size_t ) ( 200 * 1024 ) ) `

Debug and sdram_debug version of lwip_ipv4_ipv6_echo_freertos@cm4 project cannot compile in V5.37 MDK

The debug and sdram_debug version of lwip_ipv4_ipv6_echo_freertos@cm4 project cannot compile in V5.37 MDK. The location of lwip_ipv4_ipv6_echo_freertos@cm4 mdk project is: boards\evkmimxrt1170\lwip_examples\lwip_ipv4_ipv6_echo\freertos\cm4\mdk. The debug and sdram_debug version can compile successfully in V5.36 MDK. However, compile issue occurs in V5.37 MDK.

Affected platforms:

Debugger cannot connect to target board when connecting TP11 of RT1060 to J11 (pin 2) of AW-AM510 uSD wireless module

To download hands-free or handsfree_ag example to RT1060, J11 (pin 2) should only be connected to TP11 after downloading executable file to target board.

Affected platforms: evkmimxrt1060

SEGGER J-Link debugger usage problem

When an M core software is already running, it is possible to get HardFault or data verification issue during loading image into TCM by debugger.

Affected platforms: evkbmimxrt1060 mcimx93evk

Workaround: The following steps are recommended to use the J-Link debugger.

  1. Configure switch SW1301 to M core boot; low-power boot. Ensure that there is no image on the boot source.

  2. Power the board and start the debugger for use.

  3. To restart the debugger, stop the debugger, power off the board, and repeat step #2.

USB PID issue

Because the PID of all USB device examples is updated, uninstall the device drivers and then reinstall when the device (with new PID) is plugged in the first time.

Affected platforms: frdmmcxc041 frdmmcxc242 frdmmcxc444

CMSIS-PACK svd issue

CMSIS-PACK DFP installation takes a while. When installing cmsis-pack DFP, Keil MDK processes the MCU SVD file. The large size of SVD file takes considerable time to finish this conversion. During the installation, the progress appears stalled. However, it finishes after approximately 20 minutes.

Affected platforms:

littlefs_shell does not produce output

littlefs_shell example compiled by armgcc does not produce debug console output on LPCXpresso54S018M board. Root cause is unknown.

Affected platforms: lpcxpresso54s018m

Only FreeRTOS is tested for RTOS support

This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.

Affected platforms: k32w148evk

The wifi_webconfig example can get stuck after AP to client switch

The app stops uAP during switch to client, which can cause app to hang.

Affected platforms:

MCUBoot OTA examples: Encrypted XIP using IPED causes device reset

Currently, there is an issue between IPED and PKC subsystems when mbedTLS utilizes hardware acceleration. Workaround: There are two ways

1.) Disable hardware acceleration port of mbedTLS - see configuration sblconfig.h file of the ota example for more information or 2.) Place all *FUP.c files located under componentsels_pkcsrccompsin the SRAM

Examples: mcuboot_opensource, ota_mcuboot_client_wifi, ota_mcuboot_client_enet Affected toolchains: All

Affected platforms: frdmrw612, rdrw612bga

MCUBoot OTA examples: Encrypted XIP using IPED causes device reset during “Initializing WiFi connection…”

The issue is not observed in IAR toolchain and the root cause is unknown for now.

Examples: ota_mcuboot_client_wifi, ota_mcuboot_server_wifi Affected toolchains: mcux, armgcc, mdk

Affected platforms: frdmrw612, rdrw612bga

MCUBoot OTA examples: Encrypted XIP using IPED causes a hard fault during OTA update

The issue may happens when three slot mode is used in specific toolchains.

Workaround: use overwrite-only mode of encrypted XIP extension Examples: mcuboot_opensource

Affected toolchains: mcux, mdk Affected platforms: frdmrw612, rdrw612bga

Fail to set security after building connection with peer device and failed ratio is 1/10

Failed the connection with peer device.

Affected toolchains: GCC ARM, IAR, Keil, MCUXPRESSO IDE

Affected modules: 1XK_M2 1ZM_M2 2EL_M2

Affected platforms: evkmimxrt1180 evkbmimxrt1170 mcxn9xxevk mimxrt685audevk evkbimxrt1050 evkcmimxrt1060 evkmimxrt1040 evkmimxrt685 evkmimxrt595

Example hello_world_ns fails with mdk toolchain

The example hello_world_ns fails with mdk toolchain while switching to the non-secure world.

Examples: hello_world_ns, hello_world_s Affected toolchains: mdk Affected platforms: evkmimxrt1180

The wifi_webconfig example can crash while obtaining IP address

This issue can occur during DHCP handshake or other networking activity.

Examples: wifi_webconfig Affected toolchains: mdk, mcux Affected platforms: evkcmimxrt1060, evkbmimxrt1170

The aws_shadow_wifi_nxp example doesn’t work

The example ends with message: Failed to initialize file system.

Affected toolchains: mcux Affected platforms: mimxrt700evk

The flexio_spi_int_b2b flexio_spi_edma_b2b examples don’t work

Boards cannot transfer data successfully.

Affected toolchains: armgcc, mdk Affected platforms: mimxrt700evk

The cmsis_lpi2c_edma_b2b_transfer examples don’t work correctly on CM4 core.

Boards cannot transfer data successfully.

Affected toolchains: mcux Affected platforms: evkmimxrt1160, evkbmimxrt1170

The aws_examples don’t work

The example stucks during TLS connection.

Affected toolchains: mcux Affected platforms: evkmimxrt1180

The aws_shadow_enet doesn’t work

The example ends with message: xEventGroupSetBitsFromISR failed, increase configTIMER_QUEUE_LENGTH or configTIMER_TASK_PRIORITY.

Affected toolchains: mcux, mdk Affected platforms: lpcxpresso54628, lpcxpresso54s018m

The aws_shadow_wifi_serial doesn’t work

The example has problem with TLS connection.

Affected toolchains: mcux Affected platforms: lpcxpresso54s018m

The i2c_read_accel_value_transfer doesn’t work

The example has problem with identification of accelerometer.

Affected toolchains: mcux, iar, mdk, armgcc Affected platforms: lpcxpresso55s69

The spi_transfer_interrupt examples don’t work

Boards cannot transfer data successfully.

Affected toolchains: mcux Affected platforms: lpc845breakout, lpcxpresso860max

The usart_wakeup_deepsleep doesn’t work

The example doesn’t work.

Affected toolchains: mcux Affected platforms: lpcxpresso54s018

EdgeFast_Bluetooth handsfree example codec init fail

The audio codec initialization can fail during “bt aincall” command.

Workaround: Manually release the I2C bus by temporarily configuring the I2C pin as GPIO before codec initialization Examples: handsfree, handsfree_ag Affected platforms: mimxrt700evk

Examples hello_world_ns, secure_faults_ns, and secure_faults_trdc_ns have incorrect library path in GUI projects

When the affected examples are generated as GUI projects, the library linking the secure and non-secure worlds has an incorrect path set. This causes linking errors during project compilation.

Examples: hello_world_ns, hello_world_s, secure_faults_ns, secure_faults_s, secure_faults_trdc_ns, secure_faults_trdc_s

Affected toolchains: mdk, iar

Affected platforms: evk9mimx8ulp, evkmimx8ulp, evkmimxrt595, evkmimxrt685, frdmmcxn236, frdmmcxn947, frdmmcxw71, k32w148evk, mcxw72evk, kw47evk, kw45b41zevk, kw45b41zloc, lpcxpresso55s06, lpcxpresso55s16, lpcxpresso55s36, lpcxpresso55s69, mcimx93autoevk, mcimx93evk, mcimx93qsb, mcxn5xxevk, mcxn9xxevk, mimxrt685audevk, evkmimxrt1180

Workaround: In the IDE project settings for the non-secure (_ns) project, find the linked library (named hello_world_s_CMSE_lib.o, or similar, depending on the example project) and replace the path to the library with <build_directory>/<secure_world_project_folder>/<IDE>/, replacing the subdirectory names with the build directory, the secure world project name, and IDE name.

Example mbedtls_benchmark may hang on some targets on devices with ELS acceleration

Some targets of ELS accelerated devices may experience runtime issues when run with the default configuration of the mbedtls_benchmark application.

Examples: mbedtls_benchmark

Affected toolchains: All

Affected platforms: mcxn5xxevk, frdmmcxn947, mcxn9xxevk, rdrw612bga, frdmrw612

Example prince_rom does not complete successfully after the Press any key to continue message

The prince_rom example hangs after prompting the user to press a button to continue program execution.

Examples: prince_rom

Affected toolchains: iar

Affected platforms: lpcxpresso55s36

The iped example does not complete successfully

The iped example fails at multiple points.

Examples: iped

Affected toolchains: All

Affected platforms: frdmmcxn947, mcxn9xxevk, mcxn5xxevk

The bee example does not complete successfully on MCUXpresso IDE

The bee example fails when built and run via MCUXpresso IDE due to misconfigured default memory configuration.

Examples: bee

Affected toolchains: mcux

Affected platforms: evkmimxrt1015, evkmimxrt1020, evkbimxrt1050, evkmimxrt1024

The freertos_lpuart example does not complete successfully

The example hangs after console output ‘FreeRTOS LPUART driver example’.

Examples: freertos_lpuart

Affected toolchains: All

Affected platforms: kw45b41zloc

The freertos_tickless example does not complete successfully

The example does not perform as expected (Ticks do not printed on the console or the application does not wake up from the sleep mode).

Examples: freertos_tickless

Affected toolchains: All

Affected platforms: frdmrw612, evkmcimx7ulp, evkmimx8mn, evkmimx8mnddr3l, evkmimx8mq, frdmk32l3a6, kw45b41zloc

TF-M secure and EL2GO examples incorrect path in “Download extra image” with iar and mdk IDEs with Kex package

TF-M secure and EL2GO examples are missing the target path for ns binary in “extra download image” with iar and mdk IDEs

Examples: tfm_demo_s, tfm_psatest_s, tfm_regression_s, tfm_secureboot_s, el2go_agent_s, el2go_blob_test_s, el2go_import_blob_s, el2go_mqtt_demo_s Affected toolchains: mdk, iar Affected platforms: mcxn5xxevk, frdmmcxn947, mcxn9xxevk, rdrw612bga, frdmrw612 Workaround: There are two ways

1.) Flash secure and non secure bins via Jlink or SPSDK after the build with IDE and providing with correct paths of secure and non-secure binaries. or 2.) Add {target} debug/release in path of “Download extra image” for iar and for MDK in xxx_flashdownload.ini file.