Run a demo using Keil MDKVision
This section describes the steps required to build, run, and debug example applications provided in the MCUXpresso SDK.
Install CMSIS device pack
After the MDK tools are installed, Cortex Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions and flash programming algorithms. Follow these steps to install the MIMXRT104x CMSIS pack.
Download the MIMXRT1041 and MIMXRT1042 packs.
After downloading the DFP, double click to install it.
Parent topic:Run a demo using Keil MDKVision
Build an example application
Open the desired example application workspace in:
<install_dir>/boards/<board_name>/*<example\_type\>*/<application_name>/mdk
The workspace file is named as
<demo_name>.uvmpw
. For this specific example, the actual path is:<install_dir>/boards/evkmimxrt1040/demo_apps/hello_world/mdk/hello_world.uvmpw
To build the demo project, select Rebuild, highlighted in red in Figure 1.
|
|
The build completes without errors.
Parent topic:Run a demo using Keil MDKVision
Run an example application
To download and run the application, perform these steps:
This board supports the
CMSIS-DAP/mbed/DAPLink
debug probe by default. Visit os.mbed.com/handbook/Windows-serial-configuration and follow the instructions to install the Windows operating system serial driver. If running on Linux OS, this step is not required.Connect the development platform to your PC via USB cable.
Open the terminal application on the PC, such as PuTTY or TeraTerm, and connect to the debug serial port number (to determine the COM port number, see How to determine COM port). Configure the terminal with these settings:
115200 or 9600 baud rate, depending on your board (reference
BOARD_DEBUG_UART_BAUDRATE
variable in theboard.h
file)No parity
8 data bits
1 stop bit |
|
To debug the application, click load (or press the F8 key). Then, click the Start/Stop Debug Session button, highlighted in red in Figure 2. If using J-Link as the debugger, click Project option >Debug >Settings >Debug >Port, and select SW.
Note: When debugging with
jlink
, it expects onejlinkscript
file namedJLinkSettings.JLinkScript
in the folder where the uVision project files are located. For details, see SEGGER Wiki. For the contents in thisJlinkSettings.JLinkScript
, use contents inevkmimxrt1040_sdram_init.jlinkscript
.|
|
Run the code by clicking Run to start the application, as shown in Figure 3.
|
|
The `hello_world` application is now running and a banner is displayed on the terminal, as shown in [Figure 4](run_an_example_application_003.md#FIG_TEXTDISPLAY). If this is not true, check your terminal settings and connections.
|
|
Parent topic:Run a demo using Keil MDKVision