Logo
25.03.00-pvw2
MCUXpresso SDK Project v: latest
Document Release Versions
24.12.00-pvw2
24.12.00
25.03.00-pvw2

Introduction

  • MCUXpresso SDK
  • Setup

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middlewares
  • RTOS
  • Boards
    • DSC
    • Kinetis
    • LPC
    • MCX
    • i.MX RT
    • Wireless
      • FRDM-RW612
      • K32W148-EVK
      • KW45B41Z-EVK
      • KW45B41Z-LOC
      • KW47-EVK
      • KW47-LOC
      • RD-RW612-BGA
        • Overview
        • Getting Started
          • Getting Started with MCUXpresso SDK for RD-RW61X
        • Release Notes
    • i.MX

Development

  • Architecture
  • Developing with MCUXpresso SDK
  • Build And Configuration System
  • Documentation

Releases

  • Release Notes
mcuxsdk
  • Docs / 25.03.00-pvw2 »
  • Supported Boards »
  • Wireless »
  • RD-RW612-BGA »
  • Getting Started with MCUXpresso SDK for RD-RW61X
  • Open on Repo Report an issue with this page

Getting Started with MCUXpresso SDK for RD-RW61X

  • Overview

  • MCUXpresso SDK board support package folders

    • Example application structure

    • Locating example application source files

  • Run a demo using MCUXpresso IDE

    • Select the workspace location

    • Build an example application

    • Run an example application

  • Run a demo application using IAR

    • Build an example application

    • Run an example application

    • IAR RAM debugging notes

  • Run a demo using Arm GCC

    • Set up toolchain

      • Install GCC ARM Embedded tool chain

      • Install MinGW

      • Add a new system environment variable for ARMGCC_DIR

      • Install CMake

    • Build a demo application

    • Run a demo application

  • Run a demo using Keil MDK/μVision

    • Install CMSIS device pack

    • Build an example application

    • Run an example application

  • MCUXpresso IDE New Project Wizard

  • How to determine COM port

  • How to define IRQ handler in CPP files

  • Default debug interfaces

  • Updating debugger firmware

    • Updating OpenSDA firmware

    • Updating MCU-Link firmware


Copyright 2025, NXP. Last generated on Mar 06, 2025 09:10+0100; branch release/25.03.00-pvw2, revision 8403f88d835055ff0db6da35e9b065b324249514.