Toolchain introduction
The MCUXpresso SDK release for i.MX 8M Devices includes the build system to be used with some toolchains. In this chapter, the toolchain support is presented and detailed.
Compiler/Debugger
The release supports building and debugging with the toolchains listed in Table 1.
The user can choose the appropriate one for development.
Arm GCC + SEGGER J-Link GDB Server. This is a command line tool option and it supports both Windows OS and Linux OS.
IAR Embedded Workbench for Arm and SEGGER J-Link software. The IAR Embedded Workbench is an IDE integrated with editor, compiler, debugger, and other components. The SEGGER J-Link software provides the driver for the J-Link Plus debugger probe and supports the device to attach, debug, and download.
Compiler/Debugger |
Supported host OS |
Debug probe |
Tool website |
---|---|---|---|
ArmGCC/J-Link GDB server |
Windows OS/Linux OS |
J-Link Plus |
| |IAR/J-Link|Windows OS|J-Link Plus|www.iar.com
|
Download the corresponding tools for the specific host OS from the website.
Note: To support i.MX 8M Dual/8M Quad, the patch for IAR should be installed. The patch named iar_support_patch_imx8mq.zip can be used with MCUXpresso SDK. See the readme.txt in the patch for additional information about patch installation.
Parent topic:Toolchain introduction