Build an example application

To build an example application, follow these steps.

  1. Open a GCC Arm Embedded tool chain command window. To launch the window, from the Windows operating system Start menu, go to Programs -> GNU Tools Arm Embedded <version> and select GCC Command Prompt.

    |

|

  1. Change the directory to the example application project directory, which has a path similar to the following:

    <install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc
    

    For this example, the exact path is:

    <install_dir>/boards/mcimx93evk/demo_apps/hello_world/armgcc
    
  2. Type build_debug.bat on the command line or double click on the build_debug.bat file in Windows Explorer to perform the build. The output is as shown in Figure 2.

    |

|

Parent topic:Windows OS host