Bluetooth Low Energy Application Developer’s Guide
Table of Contents
- Introduction
- Prerequisites
- Bluetooth LE Host Stack Initialization and APIs
- Generic Access Profile (GAP) Layer
- Peripheral setup
- Central setup
- LE data packet length extension
- Privacy feature
- Setting PHY mode in a connection
- Data management of bonded devices
- Controller enhanced notifications
- Extended advertising
- Periodic Advertising
- Periodic Advertising with Responses (PAwR) {#periodic_advertizing_with_responses}
- Encrypted Advertising Data {#encrypted_advertising_data_0}
- Enhanced ATT
- Generic Attribute Profile (GATT) Layer
- GATT database application interface
- Creating GATT database
- Creating a Custom Profile
- Application Structure
- Folder structure
- Application main framework
- Bluetooth LE Connection Manager
- GATT database
- RTOS specifics
- Board configuration
- Bluetooth Low Energy initialization
- Bluetooth Low Energy Host Stack configuration
- Profile configuration
- Multiple connections
- Bluetooth address generation
- Repeated attempts
- Advanced Secure Mode (kw45_k32w)
- Low-Power Management
- Over the Air Programming (OTAP)
- General functionality
- Bluetooth Low Energy OTAP service-profile
- Bluetooth LE OTAP protocol
- Bluetooth Low Energy OTAP image file format
- Building Bluetooth Low Energy OTAP image file from SREC file
- Building Bluetooth Low Energy OTAP image file from BIN file
- Bluetooth Low Energy OTAP application integration
- Secured OTAP
- Creating a Bluetooth LE application when the Host Stack runs on another processor
- References
- Acronyms and abbreviations
- Note about the source code in the document
- Revision history
- Legal information {#legal-conf-ApplicationnoteUsermanualUserguideReferencemanualNon-automotive}