uart_wifi_bridge
Overview
uart_wifi_bridge
Supported Boards
FW download support monolithic
The compilation of uart_wifi_bridge is enabled monolithic by default.
How to use release mfg FW with non-monolithic configuration:
Change the monolithic macro from cmake For [RD-RW612-BGA] board mcuxsdk/examples/_boards/rdrw612bga/wifi_examples/uart_wifi_bridge/reconfig.cmake For [FRDM-RW612] board mcuxsdk/examples/_boards/rdrw612bga/wifi_examples/uart_wifi_bridge/reconfig.cmake Set CONFIG_MONOLITHIC_WIFI from 1 to 0.
Then uart_wifi_bridge build will not link FW, need to load FW separatly.
How to use release mfg FW with monolithic configuration:
Covert FW from .bin to .inc Copy the FW to mcuxsdk/components/conn_fwloader/fw_bin/ Rename the FW: rw61x_sb_ble_15d4_combo_a2.bin for CPU2 combo FW, rw61x_sb_ble_a2.bin for CPU2 single ble FW, rw61x_sb_wifi_a2.bin for CPU1 wifi FW Use mcuxsdk/components/conn_fwloader/fw_bin/script/wlan_gen_fw_incs.py to convert FW to inc files Under mcuxsdk/components/conn_fwloader/fw_bin folder: Run python script “python script/wlan_gen_fw_incs.py” The inc files will generate at mcuxsdk/components/conn_fwloader/fw_bin/inc and replace the origin inc files automatically.
Compile uart_wifi_bridge with enabled monolithc macro by default. Then uart_wifi_bridge build and link FW to a monolithic image, no need to load FW separatly.