wifi_httpsrv
Overview
The wifi_httpsrv demo application demonstrates an HTTPServer on the lwIP TCP/IP stack with FreeRTOS. The user uses an Internet browser to send a request for connection. The board acts as an HTTP server and sends a Web page back to the PC
Before building the example application select Wi-Fi module:
build from repository - select Wi-Fi module in Kconfig GUI
build from zip package - change project macro related to Wi-Fi module
WIFI_<SoC Name>_BOARD_<Module Name>, macro can be found in components\wifi_bt_module\incl\wifi_bt_module_config.h
For more information about Wi-Fi module connection see:
readme_modules.md (select supported board bellow)
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Connect the Wi-Fi module. Refer to readme_modules.md and the Supported boards section.
Set symbols WIFI_SSID and WIFI_PASSWORD to match settings of your network prior building of example.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs, it tries to connect to your network and acquire configuration form DHCP.
On success network configuration will be printed.
On the browser address bar, type IP address of the board. The browser should show a web page. The board also advertises itself using mDNS so that it can be accessed using URL http://wifi-http.local.
Please note that your system may not support mDNS out-of-the-box as it is necessary to have an mDNS resolver installed. For instance Bonjour Print Services for Windows contain such resolver. In case of Linux nss-mdns serves this purpose. Username admin and password admin is required to access “Authorization example” section of the web page.
Modifying content of static web pages
To modify content available through the web server you must complete following steps:
Modify, add or delete files in folder
boards\<board_name>\lwip_examples\lwip_httpsrv_freertos\webpage.Run the script file
middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl <directory name>to generate newhttpsrv_fs_data.c. Make sure to execute it from a folder where the filehttpsrv_fs_data.cis. For example:C:\sdk\boards\<board_name>\lwip_examples\lwip_httpsrv_freertos> C:\sdk\middleware\lwip\src\apps\httpsrv\mkfs\mkfs.pl webpage Processing file webpage/auth.html Processing file webpage/cgi.html Processing file webpage/favicon.ico Processing file webpage/help.html Processing file webpage/httpsrv.css Processing file webpage/index.html Processing file webpage/NXP_logo.png Processing file webpage/poll.html Processing file webpage/request.js Processing file webpage/ssi.shtml Processing file webpage/welcome.html Done.
Make sure the
httpsrv_fs_data.cfile has been overwritten with the newly generated content.Re-compile the HTTP server application example and download it to your board.