BDB_tsBdbEvent

The following structure contains ZigBee Base Device event information that is passed to the APP_vBdbCallback() callback function (see Events).

typedef struct
{
    BDB_teBdbEventTypee EventType;
    BDB_tuBdbEventData uEventData;
}BDB_tsBdbEvent;

where:

  • eEventType is an enumeration indicating the event type - for the possible enumerations, refer to Section 2.9.

  • uEventData is a union structure containing the event information (if any) - for a description of this structure, refer to Section 2.7.2.

Parent topic:Structures