Events
The ZigBee Base Device has a number of associated events. Some API functions (described in Functions) return immediately and the outcome of the process they invoke is later indicated with the generation of an asynchronous event. A user-defined callback function must be defined in the application to handle these events. The prototype of this callback function is as follows:
void APP_vBdbCallback(BDB_tsBdbEvent *psBdbEvent)
where psBdbEvent is a pointer to a BDB_tsBdbEvent
event structure containing the event information to be passed to the function (for this structure, see BDB_tsBdbEvent).
The enumerations for the ZigBee Base Device events are listed below.
typedef enum
{
BDB_EVENT_NONE,
BDB_EVENT_ZPSAF,
BDB_EVENT_INIT_SUCCESS,
BDB_EVENT_REJOIN_SUCCESS,
BDB_EVENT_REJOIN_FAILURE,
BDB_EVENT_NWK_STEERING_SUCCESS,
BDB_EVENT_NO_NETWORK,
BDB_EVENT_NWK_JOIN_SUCCESS,
BDB_EVENT_NWK_JOIN_FAILURE,
BDB_EVENT_APP_START_POLLING,
BDB_EVENT_NWK_FORMATION_SUCCESS,
BDB_EVENT_NWK_FORMATION_FAILURE,
BDB_EVENT_FB_HANDLE_SIMPLE_DESC_RESP_OF_TARGET,
BDB_EVENT_FB_CHECK_BEFORE_BINDING_CLUSTER_FOR_TARGET,
BDB_EVENT_FB_CLUSTER_BIND_CREATED_FOR_TARGET,
BDB_EVENT_FB_BIND_CREATED_FOR_TARGET,
BDB_EVENT_FB_GROUP_ADDED_TO_TARGET,
BDB_EVENT_FB_ERR_BINDING_FAILED,
BDB_EVENT_FB_ERR_BINDING_TABLE_FULL,
BDB_EVENT_FB_ERR_GROUPING_FAILED,
BDB_EVENT_FB_NO_QUERY_RESPONSE,
BDB_EVENT_FB_TIMEOUT,
BDB_EVENT_FB_OVER_AT_TARGET,
BDB_EVENT_LEAVE_WITHOUT_REJOIN,
}
BDB_teBdbEventType;
These events are described below.
The events with ‘FB’ in their names are used in the ‘Finding and Binding’ process and the event data is contained in the structure BDB_tsFindAndBindEvent
(see BDB_tsFindAndBindEvent).
Note: In addition, certain ZCL events are generated during the Finding and Binding process. These events are passed to the callback function BDB_vZclEventHandler(), which is supplied with the ZigBee Base Device. For these events, refer to Finding and Binding.
BDB_EVENT_ZPSAF
This event indicates that a ZigBee stack event has occurred. In this case, the
uEventData
field (of theBDB_tsBdbEvent
structure) contains aBDB_tsZpsAfEvent
structure, which itself includes theZPS_tsAfEvent
stack event structure.BDB_EVENT_INIT_SUCCESS
This event is generated when the ZigBee Base Device has been successfully initialized.
BDB_EVENT_REJOIN_SUCCESS
This event is generated when the node has successfully rejoined its previous network.
BDB_EVENT_REJOIN_FAILURE
This event is generated when the node attempts to rejoin its previous network has failed.
BDB_EVENT_NWK_STEERING_SUCCESS
This event is generated when the Network Steering process has successfully completed and the local node has broadcast either of the following messages:
Management Permit Joining message to request the network to be opened for other devices to join (this message is broadcast when the local node was already in the network before Network Steering).
Device Announce message to announce that the local node has joined the network (this message is broadcast when the local node was not in the network before Network Steering).
BDB_EVENT_NO_NETWORK
This event is generated when no open network open was discovered in a channel scan performed by a device attempting to join a network.
BDB_EVENT_NWK_JOIN_SUCCESS
This event is generated when the node has successfully joined a network.
BDB_EVENT_NWK_JOIN_FAILURE
This event is generated when the node attempted to join a network but failed.
BDB_EVENT_APP_START_POLLING
This event is generated on an End Device during the Trust Centre link key exchange procedure to instruct the application to start fast polling of its parent, in order to retrieve packets received as part of the exchange procedure.
BDB_EVENT_NWK_FORMATION_SUCCESS
This event is generated at the end of the Network Formation process when a centralized or distributed has been successfully formed by the local node.
BDB_EVENT_NWK_FORMATION_FAILURE
This event is generated at the end of the Network Formation process if the local node failed to form a network.
BDB_EVENT_FB_HANDLE_SIMPLE_DESC_RESP_OF_TARGET
This event indicates that the initiator has received a Simple Descriptor response from a target. This event can be used by the application to determine which type of device (for example: Dimmable Light, On/Off Light) the initiator is binding to. The information provided to the application is:
u8InitiatorEp u8TargetEp u16TargetAddress u16ProfileId u16DeviceId u8DeviceVersion psAfZdpEvent \(points to received Simple Descriptor\)
BDB_EVENT_FB_CHECK_BEFORE_BINDING_CLUSTER_FOR_TARGET
This event is generated just before creating a Binding table entry for a cluster. It allows the application to exclude clusters from binding by setting the
bAllowBindOrGroup
flag to FALSE (by default it is TRUE). This event can also be used when the application must perform a group binding by setting the attribute u16bdbCommissioningGroupID to a value other than 0xFFFF. Moreover, this event also allows the application to decide whether to broadcast an ‘Add Group If Identifying’ or unicast an ‘Add Group’ command. An ‘Add Group If Identifying’ is broadcast to all the identifying targets by settingbGroupCast
to TRUE. By default, this parameter is set to FALSE and allows unicasting an ‘Add Group’ request individually to all the identifying targets. The information provided to the application is:u8InitiatorEp u8TargetEp u16TargetAddress u16ClusterId bAllowBindOrGroup bGroupCast psAfZdpEvent \(points to received Simple Descriptor\)
BDB_EVENT_FB_CLUSTER_BIND_CREATED_FOR_TARGET
This event is generated per cluster for every binding or grouping created. The event may be generated more than once for the same target device. For example, when binding a color Dimmer Switch to a Dimmable Light, the event is generated twice: once for the On/Off cluster and once for the Level Control Cluster. The information provided to the application is:
u8InitiatorEp u8TargetEp u16TargetAddress u16ClusterId
BDB_EVENT_FB_BIND_CREATED_FOR_TARGET
This event is generated once all address bindings have been completed. The application can then send a ‘Stop Identifying’ command to the bound target. The information provided to the application is:
u8InitiatorEp u8TargetEp u16TargetAddress
BDB_EVENT_FB_GROUP_ADDED_TO_TARGET
This event is generated once the ‘Add Group’ or ‘Add Group If Identifying’ has been sent, in order to inform the application that grouping has been completed from the perspective of the initiator. The application can then groupcast a ‘Stop Identifying’ command to the grouped targets. The information provided to the application is:
u8InitiatorEp u8TargetEp u16GroupId u16TargetAddress psAfZdpEvent
BDB_EVENT_FB_ERR_BINDING_FAILED
This event is generated to indicate that an unexpected error has occurred while creating a Binding table entry.
BDB_EVENT_FB_ERR_BINDING_TABLE_FULL
This event is generated to inform the application that the Binding table is full and therefore the Finding and Binding process has failed. As a result, the ZigBee Base Device exits the Finding and Binding process.
BDB_EVENT_FB_ERR_GROUPING_FAILED
This event is generated to indicate that a grouping has failed, since the initiator was not able to send an ‘Add Group’ or ‘Add Group If Identifying’ request.
BDB_EVENT_FB_NO_QUERY_RESPONSE
This event indicates that the initiator did not receive an Identify Query response within BDB_FB_RESEND_IDENTIFY_QUERY_TIME (default value is 10) seconds. The information provided to the application is:
u8InitiatorEp
BDB_EVENT_FB_TIMEOUT
This event indicates that the commissioning timer expired after a period defined by the constant BDBC_MIN_COMMISSIONING_TIME (180 seconds by default). The information provided to the application is:
u8InitiatorEp
BDB_EVENT_FB_OVER_AT_TARGET
This event indicates that the Finding and Binding process has ended on the target node because the identify time reached zero or a remote node forced it to go to zero.
BDB_EVENT_LEAVE_WITHOUT_REJOIN
This event is generated when the node has been instructed to leave the network without attempting to rejoin the network.
Parent topic:ZigBee Base Device