dev_hid_mouse_lite_bm

Overview

The USB HID mouse application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a mouse. Users can see the mouse arrow moving on the PC screen according in a rectangular fashion.

System Requirements

Hardware requirements

  • Mini/micro USB cable

  • USB A to micro AB cable

  • Hardware (Tower module/base board, and so on) for a specific device

  • Personal Computer (PC)

Software requirements

  • The project files are in:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_hid_mouse//.
    For lite version, the project files are in:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_hid_mouse_lite//.

The is Bare Metal or FreeRTOS OS.

Getting Started

Hardware Settings

Set the hardware jumpers (Tower system/base module) to default settings.

Prepare the example

  1. Download the program to the target board.

  2. Connect the target board to the external power source (the example is self-powered).

  3. Power off the target board. Then power on again.

  4. Connect a USB cable between the PC and the USB device port of the board.

For detailed instructions, see the appropriate board User’s Guide.

Run the example

  1. Plug-in the device, which is running HID mouse example, into the PC. A HID-compliant mouse is enumerated in the Device Manager.

  2. The mouse arrow is moving on PC screen in the rectangular rotation.

*/

Supported Boards

  • MIMXRT1170-EVKB

  • FRDM-MCXC444

  • FRDM-K22F

  • LPCXpresso55S69

  • EVK-MIMXRT1064

  • FRDM-MCXA153

  • MIMXRT685-AUD-EVK

  • LPCXpresso51U68

  • LPCXpresso54S018

  • LPCXpresso55S16

  • FRDM-K32L2B

  • LPCXpresso54S018M

  • MIMXRT1060-EVKB

  • EVK-MIMXRT1010

  • MIMXRT1040-EVK

  • FRDM-MCXN947

  • MIMXRT1024-EVK

  • LPCXpresso55S28

  • LPCXpresso54628

  • LPCXpresso55S36

  • MCX-N5XX-EVK

  • MIMXRT1060-EVKC

  • MIMXRT1160-EVK

  • MIMXRT1180-EVK

  • FRDM-K32L2A4S

  • EVK-MIMXRT1020

  • MIMXRT700-EVK

  • FRDM-MCXA156

  • EVK-MIMXRT595

  • EVK-MIMXRT685

  • FRDM-MCXC242

  • MCX-N9XX-EVK

  • EVKB-IMXRT1050

  • RD-RW612-BGA

  • FRDM-K32L3A6

  • EVK-MIMXRT1015

  • FRDM-MCXN236

  • FRDM-RW612