dev_suspend_resume_hid_mouse
Overview
The Suspend/Resume USB HID mouse application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a mouse. Users can see the mouse arrow moving on the PC screen according in a rectangular fashion. When host releases the USB Bus, the device will enter into low power mode. The device can be waked up when resume signal is detected on the bus. Or the device can remote wake-up the host by delivering the resume signal when the remote wake-up is enabled by the host.
System Requirements
Hardware requirements
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements
The project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_suspend_resume_device_hid_mouse/ / .
For lite version, the project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_suspend_resume_device_hid_mouse_lite/ / .
The
is Bare Metal or FreeRTOS OS.
Getting Started
Hardware Settings
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
For detailed instructions, see the appropriate board User’s Guide.
Run the example
Plug-in the device, which is running Suspend/Resume HID mouse example, into the PC. A HID-compliant mouse is enumerated in the Device Manager.
The mouse arrow is moving on PC screen in the rectangular rotation.
Make sure your PC enable the USB remote wake support in BIOS.Press the sleep button to make your PC go to sleep and the USB bus becomes idle. Then the device enters into low power mode.
If the remote wake-up feature is enabled by the host, the device is waked up and delivers the resume signal when the wakeup switch is pressed. The name of wakeup switch is showed in debug console when the remote wake-up feature is enabled. For example, if the name of wakeup switch is “SW3”, the debug console output is as following.
USB device remote wakeup state: 1 USB device start suspend USB device suspended. Please Press wakeup switch(SW3) to remote wakeup the host. Remote wakeup the host. USB device start resume USB device resumed.
Or the device is waked up when the resume signal is detected on the bus.USB device remote wakeup state: 0 USB device start suspend USB device suspended. USB device start resume USB device resumed.
*/
Supported Boards
MIMXRT1170-EVKB
FRDM-K22F
LPCXpresso55S69
EVK-MIMXRT1064
MIMXRT685-AUD-EVK
MIMXRT1060-EVKB
EVK-MIMXRT1010
MIMXRT1040-EVK
MIMXRT1024-EVK
LPCXpresso55S28
LPCXpresso55S36
MIMXRT1060-EVKC
MIMXRT1160-EVK
FRDM-K32L2A4S
EVK-MIMXRT1020
MIMXRT700-EVK
FRDM-MCXA156
EVK-MIMXRT595
EVK-MIMXRT685
EVKB-IMXRT1050
FRDM-K32L3A6
EVK-MIMXRT1015
FRDM-MCXN236