Copyright 2025 NXP
SPDX-License-Identifier: BSD-3-Clause
EdgeLock 2GO Import Blob
This sample application shows how to import encrypted EdgeLock 2GO secure object blobs from flash to the Secure storage(ITS). The imported objects can then be validated by executing crypto operations.
Max Blob Size:
[KW45], [MCX W71] ‘1014 or 0x3F6’ bytes.
Additional information about EdgeLock 2GO Provisioning for MCUs can be found in AN14624 under the following link https://www.nxp.com/webapp/Download?colCode=AN14624&location=null.
Definitions
[GITHUB]: refers to the case where the MCU SDK is cloned as GitHub Repository and the EdgeLock 2GO application is build using meta build sytem. More details can be found in https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/repo.html.
[ZIP]: refers to the case whete MCU SDK is generated as ZIP package and the EdgeLock 2GO application is imported and build in one of supported IDEs. More details can be found in https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/package.html.
Prerequisites
Any serial communicator
EdgeLock 2GO secure object blobs stored in the devices flash memory
This can be achieved via the SPSDK
The following default flash location should be used to store the EdgeLock 2GO blobs:
[KW45], [MCX W71]
0x0C0000
Hardware requirements
KW45B41Z-EVK or FRDM-MCXW71 or MCXW71-EVK board
Micro-USB cable
Personal Computer
Board settings
[KW45], [MCX W71] The board must be provisioned with an OEM Auth Key Hash.
Preparing the application
[OPTIONAL] Enable the validation of imported blobs:
[GITHUB] By enabling the Kconfig symbol
VALIDATE_PSA_IMPORT_OPERATION
[ZIP] By defining
VALIDATE_PSA_IMPORT_OPERATION
as1
inmcux_config.h
This provides an example of how the imported blobs can be used. Specifically, the example demonstrates:
AES-ECB message encryption with a 256 bit key
ECDSA SHA-256 message signing
[OPTIONAL] Enable secure boot:
This feature is optional for [KW45] or [MCX W71].
The bootheader needs to be removed from the S image, it has to be merged with the NS image and the resulting image must be signed with the OEM key. Additionaly, if the application is supposed to run in the OEM CLOSED life cycle, the image needs to be encrypted with the OEM FW encryption key and loaded as an SB3.1 container.
Details on how to execute these steps can be found in the following documents:
[KW45] Application note AN14109 “Secure Boot Using the SEC Tool” (“Documentation->Secure Files” section).
[MCX W71] Application note AN14371 “Secure Boot Using the SEC Tool” (“Documentation->Secure Files” section).
[OPTIONAL] Set the flash location of the EdgeLock 2GO blobs:
In case you chose a different flash location than the default one mentioned above, you need to change two configuration options.
[GITHUB] The Kconfig symbols
BLOB_AREA
andBLOB_AREA_SIZE
[ZIP] The defines
BLOB_AREA
andBLOB_AREA_SIZE
inmcux_config.h
ATTENTION: Make sure that your choice does not overlap with any other flash regions.
Build the application:
[GITHUB] Compile the el2go_import_blob project with your desired toolchain.
[ZIP] Compile the el2go_import_blob project with your desired toolchain.
Connect the PC host to the MCU-Link USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the application to the target board:
[GITHUB]
west flash
will download the image.[ZIP] Downloading the image.
Press the reset button on the board or launch the debugger in your IDE to run the application.
Running the application
The log below shows the output of the application in the terminal window.
Importing the blobs from flash into secure-storage (ITS):
2 blob(s) imported from flash successfully
Validating the blobs (PSA crypto operation with AES master key and ECC key pair):
Validate imported blobs
Cipher encrypt passed!
ECC sign passed!