EdgeLock 2GO Import Blob (NS)

This sample application shows how to import encrypted EdgeLock 2GO secure object blobs from flash to the ITS storage. The imported objects can then be validated by executing crypto operations.

Workspace structure:

  • tfm_s_crypto_client: Project creating the static library required by the secure processing environment (S)

  • el2go_import_blob_s: Project running in the secure processing environment (S)

  • el2go_import_blob_ns: Project running in the non-secure processing environment (NS)

Additional information about EdgeLock 2GO Provisioning for MCUs can be found in AN14624 under the following link https://www.nxp.com/webapp/Download?colCode=AN14624&location=null.

Definitions

  • [GITHUB]: refers to the case where the MCU SDK is cloned as GitHub Repository and the EdgeLock 2GO application is build using meta build sytem. More details can be found in https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/repo.html.

  • [ZIP]: refers to the case whete MCU SDK is generated as ZIP package and the EdgeLock 2GO application is imported and build in one of supported IDEs. More details can be found in https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/package.html.

Prerequisites

  • Any serial communicator

  • EdgeLock 2GO secure object blobs stored in the devices flash memory

    • This can be achieved via the SPSDK

    • The following default flash location should be used to store the EdgeLock 2GO blobs:

      • [RW61X] 0x084B0000

      • [MCX-N5XX-EVK] 0x001C0000

      • [MCX-N9XX-EVK] 0x001C0000

      • [FRDM-MCXN947] 0x001C0000

      • [FRDM-MCXN236] 0x000C4000

Hardware requirements

  • FRDM-RW612, RD-RW61X-BGA, MCX-N5XX-EVK, MCX-N9XX-EVK, FRDM-MCXN947 or FRDM-MCXN236 board

  • USB-C (FRDM-RW612, FRDM-MCXN947 or FRDM-MCXN236) or Micro-USB (RD-RW61X-BGA, MCX-N5XX-EVK or MCX-N9XX-EVK) cable

  • Personal Computer

Board settings

No special settings are required.

Preparing the application

  1. [OPTIONAL] Enable the validation of imported blobs:

    • [GITHUB] By enabling the Kconfig symbol VALIDATE_PSA_IMPORT_OPERATION

    • [ZIP] By defining VALIDATE_PSA_IMPORT_OPERATION as 1 in mcux_config.h

    This provides an example of how the imported blobs can be used. Specifically, the example demonstrates:

    • AES-ECB message encryption with a 256 bit key

    • ECDSA SHA-256 message signing

  2. Enable secure boot:

    To correctly run the application on RW61X, the secure boot mode on the device needs to be enabled. For MCXN, this is optional.

    The bootheader needs to be removed from the S image, it has to be merged with the NS image and the resulting image must be signed with the OEM key. Additionaly, if the application is supposed to run in the OEM CLOSED life cycle, the image needs to be encrypted with the OEM FW encryption key and loaded as an SB3.1 container.

    Details on how to execute these steps can be found in the following documents:

  3. [OPTIONAL] Enable support for large blobs:

    In order to maximize the TF-M ITS performance, the maximum supported blob size is set to 2908 bytes. In case you want to support larger blobs (8K is the maximum size supported by PSA), you need to adjust four TF-M parameters.

    middleware/tfm/tf-m/platform/ext/target/nxp/[BOARD]/config_tfm_target.h

    #define ITS_MAX_ASSET_SIZE 3 * 0xC00
    #define CRYPTO_ENGINE_BUF_SIZE 0x4500
    

    middleware/tfm/tf-m/platform/ext/target/nxp/[BOARD]/partition/flash_layout.h

    #define TFM_HAL_ITS_SECTORS_PER_BLOCK (3)
    

    middleware/tfm/tf-m/platform/ext/target/nxp/[BOARD]/partition/region_defs.h

    #define NS_HEAP_SIZE (0x6000)
    
  4. [OPTIONAL] Set the flash location of the EdgeLock 2GO blobs:

    In case you chose a different flash location than the default one mentioned above, you need to change two configuration options.

    • [GITHUB] The Kconfig symbols BLOB_AREA and BLOB_AREA_SIZE

    • [ZIP] The defines BLOB_AREA and BLOB_AREA_SIZE in mcux_config.h

    Also, you need to adjust two TF-M parameters.

    middleware/tfm/tf-m/platform/ext/target/nxp/[BOARD]/partition/flash_layout.h

    #define TFM_EL2GO_NV_DATA_IMPORT_ADDR (0x084A0000)
    #define TFM_EL2GO_NV_DATA_IMPORT_SIZE (0x00060000)
    

    ATTENTION: Make sure that your choice does not overlap with any other flash regions.

  5. Build the application:

    • [GITHUB] Compile the el2go_import_blob_ns project with your desired toolchain using --sysbuild.

    • [ZIP] First compile the el2go_import_blob_s project and then the el2go_import_blob_ns project.

  6. Connect the USB-C (FRDM-RW612, FRDM-MCXN947) or Micro-USB (RD-RW61X-BGA, MCX-N5XX-EVK or MCX-N9XX-EVK) cable to the PC host and the MCU-Link USB port (J10 [FRDM-RW612], J7 [RD-RW61X-BGA], J5 [MCX-N5XX-EVK or MCX-N9XX-EVK] or J17 [FRDM-MCXN947]) on the board.

  7. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  8. Download the application to the target board:

    • [GITHUB] west flash will download both the S and the NS image.

    • [ZIP] Downloading the S image will also download the NS image.

  9. Press the reset button on the board or launch the debugger in your IDE to run the application.

Running the application

The log below shows the output of the application in the terminal window.

Booting the S project (TF-M initialization):

Booting TF-M v2.1.1
[WRN] This device was provisioned with dummy keys. This device is NOT SECURE
[Sec Thread] Secure image initializing!
TF-M Float ABI: Hard
Lazy stacking enabled
[INF][PS] Encryption alg: 0x5500100

Jumping to the NS project, importing the blobs from flash into TF-M ITS:

2 blob(s) imported from flash successfully

Validating the blobs (PSA crypto operation with AES master key and ECC key pair):

Validate imported blobs

Cipher encrypt passed!

ECC sign passed!