ZigBee 3.0 SDK

The ZigBee 3.0 SDK provides the stack and API software resources needed to develop ZigBee 3.0 applications for the JN518x and K32W041/K32W061/K32W1/MCXW71/MCXW72/RW612 devices and includes:

  • ZigBee PRO and IEEE 802.15.4 stack software

  • ZigBee PRO APIs

  • ZigBee Base Device Behavior (BDB) APIs

  • ZigBee Cluster Library (ZCL) APIs

  • Connectivity Framework APIs

  • ZPS Configuration Editor

  • Integrated Peripherals APIs and Board APIs

NXP-specific tools have been devised for MCUXpresso, including the ZPS Configuration Editor, which is provided as an Eclipse plug-in. This tool is used to set network parameters and is described in Chapter 13, ZPS Configuration Editor.

This ZigBee 3.0 SDK contains device-specific plug-ins for the MCUXpresso platform.

MCUXpresso must be installed before the ZigBee 3.0 SDK. Refer to Section 5.1.1, Development platform for information on this toolchain.

Parent topic:Development environment and resources