ZPS_eAplAfBoundAckDataReq
ZPS\_teStatus ZPS\_eAplAfBoundAckDataReq(
PDUM\_thAPduInstance hAPduInst,
uint16 u16ClusterId,
uint8 u8SrcEndpoint,
ZPS\_teAplAfSecurityMode eSecurityMode,
uint8 u8Radius,
uint8 *pu8SeqNum);
Description
This function submits a request to send data to all nodes/endpoints to which the source node/endpoint has been previously bound (using the binding functions, described in Section 9.1.3) and requires an acknowledgment to be returned by the remote node(s) once the data reaches its destination(s). You must specify the local endpoint and output cluster from which the data originates (the cluster must be in the Simple descriptor for the endpoint).
The data is sent in an Application Protocol Data Unit (APDU) instance, which can be allocated using the PDUM function PDUM_hAPduAllocateAPduInstance() and then written to using PDUM_u16APduInstanceWriteNBO().
If the APDU size is larger than the maximum packet size allowed on the network, the APDU can be broken up into fragments (NPDUs) for transmission. To enable this fragmentation, set the ZigBee network parameter Maximum Number of Transmitted Simultaneous Fragmented Messages to a non-zero value.
Once the sent data reaches its final destination node(s), a ZPS_EVENT_BIND_REQUEST_SERVER event is generated on the local node. This event reports the status of the bound transmission, including the number of bound endpoints for which the transmission has failed.
Security (encyption/decryption) can be applied to the APDU, where this security can be implemented at the Application layer or the network (ZigBee) layer, or both.
Parent topic:ZPS_eAplAfBoundAckDataReq
Parameters
hAPduInst: Handle of APDU instance to be sent
u16ClusterId: Identifier of relevant output cluster on source endpoint
u8SrcEndpoint: Source endpoint number (1-240) on local node
eSecurityMode: Security mode for data transfer:
ZPS_E_APL_AF_UNSECURE (no security enabled)
ZPS_E_APL_AF_SECURE (Application-level security using link key and network key)
ZPS_E_APL_AF_SECURE_NWK (Network-level security using network key)
ZPS_E_APL_AF_SECURE | ZPS_E_APL_AF_EXT_NONCE (Application-level security using link key and network key with the extended NONCE included in the frame)
ZPS_E_APL_AF_WILD_PROFILE (May be combined with above flags using OR operator. Sends the message using the wildcard profile (0xFFFF) instead of the profile in the associated Simple descriptor)
u8Radius: Maximum number of hops permitted to destination node (zero value specifies that default maximum is to be used)
*pu8SeqNum: Pointer to location to receive sequence number assigned to data transfer request. If not required, set to NULL.
Parent topic:ZPS_eAplAfBoundAckDataReq
Returns
ZPS_E_SUCCESS
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplAfBoundAckDataReq
Parent topic:Data Transfer functions