ZPS_eAplZdoGroupAllEndpointRemove

ZPS_teStatus ZPS_eAplZdoGroupAllEndpointRemove(
                            uint8 u8DstEndpoint);

Description

This function requests that the specified endpoint (on the local node) is removed from all groups to which it currently belongs.

Information on the endpoints in a group can be obtained from the Group Address table in the AIB (which can be accessed using the function ZPS_psAplAibGetAib()).

Parent topic:ZPS_eAplZdoGroupAllEndpointRemove

Parameters

u8DstEndpoint Number of destination endpoint (1-240) on local node

Parent topic:ZPS_eAplZdoGroupAllEndpointRemove

Returns

  • ZPS_E_SUCCESS (endpoint successfully removed from all groups)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdoGroupAllEndpointRemove

Parent topic:Addressing functions