ZPS_eAplZdoGroupEndpointRemove
ZPS_teStatus ZPS_eAplZdoGroupEndpointRemove(
uint16 u16GroupAddr,
uint8 u8DstEndpoint);
Description
This function requests that the specified endpoint (on the local node) is removed from the group with the specified group address.
If you wish to remove an endpoint from all groups to which it belongs, use the functionZPS_eAplZdoGroupAllEndpointRemove().
Information on the endpoints in a group can be obtained from the Group Address table in the AIB (which can be accessed using the function ZPS_psAplAibGetAib()).
Parent topic:ZPS_eAplZdoGroupEndpointRemove
Parameters
u16GroupAddr: 16-bit group address
u8DstEndpoint: Number of destination endpoint (1-240) on local node
Parent topic:ZPS_eAplZdoGroupEndpointRemove
Returns
ZPS_E_SUCCESS (endpoint successfully removed from group)
APS return codes, listed and described in Section 111.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoGroupEndpointRemove
Parent topic:Addressing functions