ZPS_eAplZdoUnbindGroup

ZPS_teStatus ZPS_eAplZdoUnbindGroup(
      uint16 u16ClusterId,
      uint8 u8SrcEndpoint,
      uint16 u16DstGrpAddr);

Description

This function requests an existing binding to be removed between an endpoint on the local node and a group of endpoints on remote nodes, where this binding was created using the function ZPS_eAplZdoBindGroup(). The source endpoint and cluster must be specified, as well as the destination nodes/endpoints for the binding, which must be specified using a 16-bit group address.

The binding is removed from the binding table on the local node.

Parent topic:ZPS_eAplZdoUnbindGroup

Parameters

u16ClusterId Identifier of bound cluster on source node

u8SrcEndpoint Number of bound endpoint (1-240) on source node

u16DstGrpAddr 16-bit group address of bound destination group

Parent topic:ZPS_eAplZdoUnbindGroup

Returns

  • ZPS_E_SUCCESS (binding successfully removed)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdoUnbindGroup

Parent topic:Network deployment functions