ZPS_eAplZdpActiveEpRequest

ZPS\_teStatus ZPS\_eAplZdpActiveEpRequest\(
    PDUM\_thAPduInstance hAPduInst,
    ZPS\_tuAddress uDstAddr,
    bool bExtAddr,
    uint8 *pu8SeqNumber,
    ZPS\_tsAplZdpActiveEpReq *psZdpActiveEpReq);

Description

This function requests a list of the active endpoints on a remote node. The function sends an Active_EP_req request either to the relevant node or to another node that may hold the required information in its primary discovery cache.

The network address of the node of interest must be specified in the request, which is represented by the structure below (further detailed in Section 9.2.2.11).

typedef struct {

uint16 u16NwkAddrOfInterest;

} ZPS_tsAplZdpActiveEpReq;

The endpoint list is received in an Active_EP_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpActiveEpRsp(detailed in Section 9.2.3.10).

Parent topic:ZPS_eAplZdpActiveEpRequest

Parameters

  • hAPduInst: Handle of APDU instance in which request is sent

  • uDstAddr: Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr: Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • *pu8SeqNumber: Pointer to sequence number of request

  • *psZdpActiveEpReq: Pointer to request (see above)

Parent topic:ZPS_eAplZdpActiveEpRequest

Returns

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpActiveEpRequest

Parent topic:Service Discovery functions