ZPS_eAplZdpBackupSourceBindRequest
ZPS_teStatus ZPS_eAplZdpBackupSourceBindRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpBackupSourceBindReq
*psZdpBackupSourceBindReq);
Description
This function requests that a back-up of the locally held source binding table is performed on a remote node. This source binding table contains entries only relevant to the local node. The function must be called from a node with a primary binding table cache and the destination node of the request must hold the corresponding back-up binding table cache.
Note: This function is provided in the NXP ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED
.
This request must include the source binding table entries to be backed up. The request is represented by the structure below (further detailed in Section 9.2.2.31).
typedef struct {
uint16 u16SourceTableEntries; uint16 u16StartIndex;
uint16 u16SourceTableListCount;
/* Rest of message is variable length */ uint64* pu64SourceAddress;
} ZPS_tsAplZdpBackupSourceBindReq;
On receiving the request, the remote node saves the new source binding table, if possible, overwriting existing entries. If the new table is longer than the previous one, as many extra entries as possible will be saved.
The remote node replies with a Backup_Source_Bind_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpBackupSourceBindRsp
(detailed in Section 9.2.3.31).
Parent topic:ZPS_eAplZdpBackupSourceBindRequest
Parameters
hAPduInst Handle of APDU instance in which request is sent.
uDstAddr Address of destination node of request (can be 16- or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpBackupSourceBindReqPointer to request (see above)
Parent topic:ZPS_eAplZdpBackupSourceBindRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpBackupSourceBindRequest
Parent topic:Binding functions