ZPS_eAplZdpExtendedSimpleDescRequest
ZPS\_teStatus ZPS\_eAplZdpExtendedSimpleDescRequest\(
PDUM\_thAPduInstance hAPduInst,
ZPS\_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS\_tsAplZdpExtendedSimpleDescReq
*psZdpExtendedSimpleDescReq);
Description
This function requests a cluster list for a specific endpoint on the node with a particular network address. The function should be called if the endpoint has more input or output clusters than could be included in the response to ZPS_eAplZdpSimpleDescRequest(). The function sends an Extended_Simple_Desc_req request either to the relevant node or to another node that may hold the required information in its primary discovery cache.
The network address of the node of interest and the relevant endpoint on the node must be specified in the request, which is represented by the structure below (further detailed in Section 9.2.2.7).
typedef struct { uint16 u16NwkAddr; uint8 u8EndPoint;
uint8 u8StartIndex;
} ZPS_tsAplZdpExtendedSimpleDescReq;
This structure allows you to specify the first input/output cluster of interest in the endpoint’s input and output cluster lists. Thus, this should normally be the cluster after the last one reported following a call to ZPS_eAplZdpSimpleDescRequest().
The required cluster information is received in a Extended_Simple_Desc_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpExtendedSimpleDescRsp
(detailed in Section 9.2.3.6).
Parent topic:ZPS_eAplZdpExtendedSimpleDescRequest
Parameters
hAPduInst: Handle of APDU instance in which request is sent
uDstAddr: Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)
bExtAddr: Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
*pu8SeqNumber: Pointer to sequence number of request
*psZdpExtendedSimpleDescReq: Pointer to request (see above)
Parent topic:ZPS_eAplZdpExtendedSimpleDescRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpExtendedSimpleDescRequest
Parent topic:Service Discovery functions