ZPS_eAplZdpFindNodeCacheRequest

ZPS\_teStatus ZPS\_eAplZdpFindNodeCacheRequest\(
  PDUM\_thAPduInstance hAPduInst,
  uint8 *pu8SeqNumber,
  ZPS\_tsAplZdpFindNodeCacheReq
            *psZdpFindNodeCacheReq);

Description

This function can be used to search for nodes in the network that hold ‘discovery information’ about a particular node. The function broadcasts a Find_node_cache_reqrequest to the network.

This request includes the network and IEEE addresses of the node of interest. The request is represented by the structure below (further detailed in Section 8.2.2.21).

typedef struct {
    uint16 u16NwkAddr;
    uint64 u64IeeeAddr;
} ZPS_tsAplZdpFindNodeCacheReq;

On receiving the request, a remote node first checks whether it has a primary discovery cache, or is the specified node itself. If either is the case, it checks whether it holds the required information and, if this is the case, replies with a Find_node_cache_rspresponse. This response should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpFindNodeCacheRsp(detailed in Section 8.2.3.20).

Only nodes that hold the required information respond to the request.

Parent topic:ZPS_eAplZdpFindNodeCacheRequest

Parameters

  • hAPduInst: Handle of APDU instance in which request is sent.

  • *pu8SeqNumber: Pointer to sequence number of request

  • *psZdpFindNodeCacheReq: Pointer to request (see above)

Parent topic:ZPS_eAplZdpFindNodeCacheRequest

Returns

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpFindNodeCacheRequest

Parent topic:Service Discovery functions