ZPS_eAplZdpMgmtRtgRequest

ZPS_teStatus ZPS_eAplZdpMgmtRtgRequest(
        PDUM_thAPduInstance hAPduInst,
        ZPS_tuAddress uDstAddr,
        bool bExtAddr,
        uint8 *pu8SeqNumber,
        ZPS_tsAplZdpMgmtRtgReq *psZdpMgmtRtgReq);

Description

This function requests a remote node to provide the contents of its Routing table. The destination node of this request must be a Router or the Coordinator.

This request must specify the index of the first entry in the Routing table to report. The request is represented by the structure below (further detailed in Section 8.2.2.35).

typedef struct {

uint8 u8StartIndex;

} ZPS_tsAplZdpMgmtRtgReq;

The remote node replies with a Mgmt_Rtg_rsp response containing the required information, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtRtgRsp(detailed in Section 8.2.3.35).

Parent topic:ZPS_eAplZdpMgmtRtgRequest

Parameters

  • hAPduInst Handle of APDU instance in which request is sent.

  • uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)

  • bExtAddr Type of destination address:

    • TRUE: 64-bit IEEE (MAC) address

    • FALSE: 16-bit network address

  • * pu8SeqNumber Pointer to sequence number of request

  • * psZdpMgmtRtgReq Pointer to request (see above)

Parent topic:ZPS_eAplZdpMgmtRtgRequest

Returns

  • ZPS_E_SUCCESS (request successfully sent)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_eAplZdpMgmtRtgRequest

Parent topic:ZPS_eAplZdpMgmtBindRequest

Parent topic:Network Management Services functions