ZPS_vAplAfSetEndpointState
ZPS\_teStatus ZPS\_eAplAfSetEndpointState\(
uint8 u8Endpoint,
bool bEnabled);
Description
This function puts the specified endpoint on the local node into the specified state (enabled or disabled).
Parent topic:ZPS_vAplAfSetEndpointState
Parameters
u8Endpoint: Endpoint number (on local node)
bEnabled: State in which to put endpoint, one of:
TRUE: enable endpoint
FALSE: disable endpoint
Parent topic:ZPS_vAplAfSetEndpointState
Returns
ZPS_E_SUCCESS (endpoint state successfully set)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_vAplAfSetEndpointState
Parent topic:Endpoint functions