Functions

The following On/Off cluster functions are provided in the NXP implementation of the ZCL:

  1. eCLD_OnOffCreateOnOff

  2. _OnOffCommandSend

  3. eCLD_OnOffCommandOffWithEffectSend

  4. eCLD_OnOffCommandOnWithTimedOffSend

eCLD_OnOffCreateOnOff

teZCL_Status eCLD_OnOffCreateOnOff(
    tsZCL_ClusterInstance *psClusterInstance,
    bool_t bIsServer,
    tsZCL_ClusterDefinition *psClusterDefinition,
    void *pvEndPointSharedStructPtr,
    uint8 *pu8AttributeControlBits,
    tsCLD_OnOffCustomDataStructure
*psCustomDataStructure);

Description

This function creates an instance of the On/Off cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.

The function must be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates an On/Off cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.

Note: Do not call this function for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.

When used, this function must be the first On/Off cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.

The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate to the total number of attributes supported by the On/Off cluster. The function initialises the array elements to zero.

Parameters

  • psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initialising individual structure fields.

  • bIsServer: Type of cluster instance (server or client) to be created:

    • TRUE - server

    • FALSE - client

  • psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the On/Off cluster. This parameter can refer to a pre-filled structure called sCLD_OnOff which is provided in the OnOff.h file.

  • pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type tsCLD_OnOff which defines the attributes of On/Off cluster. The function initialises the attributes with default values.

  • pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above)

  • psCustomDataStructure: Pointer to a structure containing the storage for internal functions of the cluster (see Section 14.8.1)

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

Parent topic:Functions

eCLD_OnOffCommandSend

teZCL_Status eCLD_OnOffCommandSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    teCLD_OnOff_Command eCommand);

Description

This function sends a custom command instructing the target device to perform the specified operation on itself: switch off, switch on, toggle (on-to-off or off-to-on), or switch on with settings retrieved from the global scene, This last option (On with Recall Global Scene) is described in Section 14.6 and, if used, must be enabled in the compile-time options on the server (target), as indicated in Section 14.10.

The device receiving this message generates a callback event on the endpoint on which the On/Off cluster was registered.

If the Level Control cluster (see Chapter 16) is also used on the target device, an ‘On’ or ‘Off’ command can be implemented with a transition effect, as follows:

  • If the optional Level Control ‘On Transition Time’ attribute is enabled, an ‘On’ command results in a gradual transition. This transition is from the ‘off’ level to the ‘on’ level over the time-interval specified in the attribute.

  • If the optional Level Control ‘Off Transition Time’ attribute is enabled, an ‘Off’ command results in a gradual transition from the ‘on’ level to the ‘off’ level over the time-interval specified in the attribute.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request

  • eCommand: Command code, one of the following:

    • E_CLD_ONOFF_CMD_OFF

    • E_CLD_ONOFF_CMD_ON

    • E_CLD_ONOFF_CMD_TOGGLE

    • E_CLD_ONOFF_CMD_ON_RECALL_GLOBAL_SCENE

    • E_CLD_ONOFF_CMD_TOGGLE

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_OnOffCommandOffWithEffectSend

teZCL_Status eCLD_OnOffCommandOffWithEffectSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_OnOff_OffWithEffectRequestPayload *psPayload);

Description

This function sends a custom ‘Off With Effect’ command instructing the target lighting device to switch off one or more lights with the specified effect, which can be one of:

  • fade (in two phases or no fade)

  • rise and fall

Each of these effects is available in variants. The required effect and variant are specified in the command payload. For the payload details, refer to “Off With Effect Request Payload “.

The device receiving this message generates a callback event on the endpoint on which the On/Off cluster was registered.

Following a call to this function, the light settings on the target device are saved to a global scene, after which the attribute bGlobalSceneControl is set to FALSE - for more details, refer to Section 14.6.

If used, the ‘Off With Effect’ command must be enabled in the compile-time options on both the client and server, as described in Section 14.10.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 14.8.2).

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

eCLD_OnOffCommandOnWithTimedOffSend

teZCL_Status eCLD_OnOffCommandOnWithTimedOffSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_OnOff_OnWithTimedOffRequestPayload
    *psPayload);

Description

This function sends a custom ‘On With Timed Off’ command instructing the target lighting device to switch on one or more lights for a timed period and then switch them off. In addition, a waiting time can be implemented after switch-off, during which the lights cannot be switched on again.

The following functionality must be specified in the command payload:

  • Time for which the lights must remain on.

  • Waiting time during which switched-off lights cannot be switched on again.

  • Whether this command can be accepted at any time (outside the waiting time) or only when a light is on.

For the payload details, refer to “On With Timed Off Request Payload”.

The device receiving this message generates a callback event on the endpoint on which the On/Off cluster was registered.

If used, the ‘On With Timed Off’ command must be enabled in the compile-time options on both the client and server, as described in Section 14.10.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 14.8.2).

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions

Parent topic:On/Off Cluster