eCLD_ScenesCommandEnhancedViewSceneRequestSend

teZCL_Status eCLD_ScenesCommandEnhancedViewSceneRequestSend(
    uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ScenesEnhancedViewSceneRequestPayload
*psPayload);

Description

This function sends an Enhanced View Scene command to a remote device, requesting information on a particular scene on the destination endpoint. The returned information includes the finer transition time configured with the function eCLD_ScenesCommandEnhancedAddSceneRequestSend(). The relevant scene ID is specified in the command payload. Note that this command can only be sent to an individual device/endpoint and not to a group address.

The device receiving this message generates a callback event on the endpoint on which the Scenes cluster was registered and generates an Enhanced View Scene response containing the relevant information (see Section 13.7.3).

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address type eZCL_AMBOUND.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 13.7.2)

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions