ZCL Structures
This chapter details the structures that are not specific to any particular ZCL cluster.
Note: Cluster-specific structures are detailed in the chapters for the respective clusters.
General Structures
tsZCL_EndPointDefinition
This structure defines the endpoint for an application:
struct tsZCL_EndPointDefinition
{
uint8 u8EndPointNumber;
uint16 u16ManufacturerCode;
uint16 u16ProfileEnum;
bool_t bIsManufacturerSpecificProfile;
uint16 u16NumberOfClusters;
tsZCL_ClusterInstance *psClusterInstance;
bool_t bDisableDefaultResponse;
tfpZCL_ZCLCallBackFunction pCallBackFunctions;
};
Where:
u8EndPointNumber
is the endpoint number between 1 and 240 (0 is reserved)u16ManufacturerCode
is the manufacturer code (only valid whenbIsManufacturerSpecificProfile
is set to TRUE)u16ProfileEnum
is the ZigBee application profile IDbIsManufacturerSpecificProfile
indicates whether the application profile is proprietary (TRUE) or from the ZigBee Alliance (FALSE)u16NumberOfClusters
is the number of clusters on the endpointpsClusterInstance
is a pointer to an array of cluster instance structuresbDisableDefaultResponse
can be used to disable the requirement for default responses to be returned for commands sent from the endpoint (TRUE=disable, FALSE=enable)pCallBackFunctions
is a pointer to the callback functions for the endpoint
Parent topic:General Structures
tsZCL_ClusterDefinition
This structure defines a cluster used on a device:
typedef struct
{
uint16 u16ClusterEnum;
bool_t bIsManufacturerSpecificCluster;
uint8 u8ClusterControlFlags;
uint16 u16NumberOfAttributes;
tsZCL_AttributeDefinition *psAttributeDefinition;
tsZCL_SceneExtensionTable *psSceneExtensionTable;
#ifdef ZCL_COMMAND_DISCOVERY_SUPPORTED
uint8 u8NumberOfCommands;
tsZCL_CommandDefinition *psCommandDefinition;
#endif
} tsZCL_ClusterDefinition;
Where:
u16ClusterEnum
is the Cluster ID.bIsManufacturerSpecificCluster
indicates whether the cluster is specific to a manufacturer (proprietary):TRUE - proprietary cluster
FALSE - ZigBee cluster
u8ClusterControlFlags is a bitmap containing control bits in two parts, as follows:
Bits |
Description |
Values |
---|---|---|
0 - 3 |
Type of security |
Indicates the type of security key used via one of the following |
Bits |
Description |
Values |
---|---|---|
0 - 3 |
Type of security |
Indicates the type of security key used via one of the following teZCL_ZCLSend Security enumerations (see Section 7.1.6): E_ZCL_SECURITY_NETWORK, E_ZCL_SECURITY_APPLINK |
4 - 7 |
Cluster mirror |
Used internally to indicate whether the cluster is mirrored, as follows: |
u16NumberOfAttributes
indicates the number of attributes in the cluster.psAttributeDefinition
is a pointer to an array of attribute definition structures - see Section 6.1.3.psSceneExtensionTable
is a pointer to a structure containing a Scene Extension table - see Section 6.1.20.The following optional pair of fields are related to the Command Discovery feature (see Section 2.9):
u8NumberOfCommands
is the number of supported commands in the Command Definition table (see below).psCommandDefinition
is a pointer to a Command Definition table which contains a list of the commands supported by the cluster - each entry of the table contains the details of a supported command in atsZCL_CommandDefinition
structure (see Section 6.1.19).
Parent topic:General Structures
tsZCL_AttributeDefinition
This structure defines an attribute used in a cluster:
struct tsZCL_AttributeDefinition
{
uint16 u16AttributeEnum;
uint8 u8AttributeFlags;
teZCL_ZCLAttributeType eAttributeDataType;
uint16 u16OffsetFromStructBase;
uint16 u16AttributeArrayLength;
};
Where:
u16AttributeEnum
is the Attribute ID.u8AttributeFlags
is a 5-bit bitmap indicating the accessibility of the attribute (for details of the access types, refer to Section 2.3.1) - a bit is set to ‘1’ if the corresponding access type is supported, as follows:
Bit |
Access Type |
---|---|
0 |
Read |
1 |
Write |
2 |
Reportable |
3 |
Scene |
4 |
Global |
5-7 |
Reserved |
eAttributeDataType
is the data type of the attribute - see Section 7.1.3.u16O``ffsetFromStructBase
is the offset of the attribute’s location from the start of the cluster.u16AttributeArrayLength
is the number of consecutive attributes of the same type.
Parent topic:General Structures
tsZCL_Address
This structure is used to specify the addressing mode and address for a communication with a remote node:
typedef struct PACK
{
teZCL_AddressMode eAddressMode;
union {
zuint16 u16GroupAddress;
zuint16 u16DestinationAddress;
zuint64 u64DestinationAddress;
teAplAfBroadcastMode eBroadcastMode;
} uAddress;
} tsZCL_Address;
Where:
eAddressMode
is the addressing mode to be used (see Section 7.1.1).uAddress
is a union containing the necessary address information (only one of the following must be set, depending on the addressing mode selected):u16GroupAddress
is the 16-bit group address for the target nodes.u16DestinationAddress
is the 16-bit network address of the target.u64DestinationAddress
is the 64-bit IEEE/MAC address of the target.eBroadcastMode
is the required broadcast mode (see Section 7.1.2).
Parent topic:General Structures
tsZCL_AttributeReportingConfigurationRecord
This structure contains the configuration record for automatic reporting of an attribute.
typedef struct
{
uint8 u8DirectionIsReceived;
teZCL_ZCLAttributeType eAttributeDataType;
uint16 u16AttributeEnum;
uint16 u16MinimumReportingInterval;
uint16 u16MaximumReportingInterval;
uint16 u16TimeoutPeriodField;
tuZCL_AttributeReportable uAttributeReportableChange;
} tsZCL_AttributeReportingConfigurationRecord;
Where:
u8DirectionIsReceived
indicates whether the record configures how attribute reports can be received or sent:0x00: Configures how attribute reports are sent by the server - the following fields are included in the message payload:
eAttributeDataType
,u16MinimumReportingInterval
,u16MaximumReportingInterval
,uAttributeReportableChange
0x01: Configures how attribute reports are received by the client -
u16TimeoutPeriodField
is included in the message payload.
eAttributeDataType
indicates the data type of the attribute.u16AttributeEnum
is the identifier of the attribute to which the configuration record relates.u``16MinimumReportingInterval
is the minimum time-interval, in seconds, between consecutive reports for the attribute - the value 0x0000 indicates no minimum (REPORTING_MINIMUM_LIMIT_NONE).u16MaximumReportingInterval
is the time-interval, in seconds, between consecutive reports for periodic reporting - the following special values can also be set:0x0000 indicates that periodic reporting is to be disabled for the attribute (REPORTING_MAXIMUM_PERIODIC_TURNED_OFF).
0xFFFF indicates that automatic reporting is to be completely disabled for the attribute (REPORTING_MAXIMUM_TURNED_OFF).
u16TimeoutPeriodField
is the timeout value, in seconds, for an attribute report - if the time elapsed since the last report exceeds this value (without receiving another report), it may be assumed that there is a problem with the attribute reporting - the value 0x0000 indicates that no timeout will be applied (REPORTS_OF_ATTRIBUTE_NOT_SUBJECT_TO_TIMEOUT).uAttributeReportableChange
is the minimum change in the attribute value that causes an attribute report to be issued.
Note: For successful attribute reporting, the timeout on the receiving client must be set to a higher value than the maximum reporting interval for the attribute on the sending server.
Parent topic:General Structures
tsZCL_AttributeReportingConfigurationResponse
This structure contains information from a ‘configure reporting’ response.
typedef struct
{
teZCL_CommandStatus eCommandStatus;
tsZCL_AttributeReportingConfigurationRecord
sAttributeReportingConfigurationRecord;
}tsZCL_AttributeReportingConfigurationResponse;
Where:
eCommandStatus
is an enumeration representing the status from the response (see Section 7.1.4).sAttributeReportingConfigurationRecord
is a configuration record structure (see Section 6.1.5), but only the fieldsu16AttributeEnum
andu8DirectionIsReceived
are used in the response.
Parent topic:General Structures
tsZCL_AttributeReadReportingConfigurationRecord
This structure contains the details of a reporting configuration query for one attribute, to be included in a ‘read reporting configuration’ command:
typedef struct
{
uint8 u8DirectionIsReceived;
uint16 u16AttributeEnum;
} tsZCL_AttributeReadReportingConfigurationRecord;
Where:
u8DirectionIsReceived
specifies whether the required reporting configuration information details how the attribute reports are received or sent.0x00: Specifies that required information details how a report is sent by the server.
0x01: Specifies that required information details how a report is received by the client.
u16AttributeEnum
is the identifier of the attribute to which the required reporting configuration information relates.
Parent topic:General Structures
tsZCL_IndividualAttributesResponse
This structure is contained in a ZCL event of type E_ZCL_CBET_READ_INDIVIDUAL_ATTRIBUTE_RESPONSE (see Section):
typedef struct PACK {
uint16 u16AttributeEnum;
teZCL_ZCLAttributeType eAttributeDataType;
teZCL_CommandStatus eAttributeStatus;
void *pvAttributeData;
} tsZCL_IndividualAttributesResponse;
Where:
u16AttributeEnum
identifies the attribute that has been read (the relevant enumerations are listed in the ‘Enumerations’ section of each cluster-specific chapter).eAttributeDataType
is the ZCL data type of the read attribute (see Section 7.1.3).eAttributeStatus
is the status of the read operation (0x00 for success or an error code - see Section 7.1.4 for enumerations).pvAttributeData
is a pointer to the read attribute data which (if the read was successful) has been inserted by the ZCL into the shared device structure.
The above structure is contained in the tsZCL_CallBackEvent
event structure, detailed in Section 6.2, when the field eEventType
is set to E_ZCL_CBET_READ_INDIVIDUAL_ATTRIBUTE_RESPONSE.
Parent topic:General Structures
tsZCL_DefaultResponse
This structure is contained in a ZCL event of type E_ZCL_CBET_DEFAULT_RESPONSE (see Section):
typedef struct PACK {
uint8 u8CommandId;
uint8 u8StatusCode;
} tsZCL_DefaultResponse;
Where:
u8CommandId
is the ZCL identifier of the command that triggered the default response messageu8StatusCode
is the status code from the default response message (0x00 for OK or an error code defined in the ZCL Specification - see Section 4.2)
The above structure is contained in the tsZCL_CallBackEvent
event structure, detailed in Section 6.2, when the field eEventType
is set to E_ZCL_CBET_DEFAULT_RESPONSE.
Parent topic:General Structures
tsZCL_AttributeDiscoveryResponse
This structure contains details of an attribute reported in a ‘discover attributes’ response. It is contained in a ZCL event of type E_ZCL_CBET_DISCOVER_INDIVIDUAL_ATTRIBUTE_RESPONSE.
typedef struct
{
bool_t bDiscoveryComplete;
uint16 u16AttributeEnum;
teZCL_ZCLAttributeType eAttributeDataType;
} tsZCL_AttributeDiscoveryResponse;
where:
bDiscoveryComplete
indicates whether this is the final attribute from a ‘discover attributes’ to be reported:TRUE - final attribute
FALSE - not final attribute
u16AttributeEnum
is the identifier of the attribute being reportedeAttributeDataType
indicates the data type of the attribute being reported (see Section 7.1.3)
The above structure is contained in the tsZCL_CallBackEvent
event structure, detailed in Section 6.2, when the field eEventType
is set to E_ZCL_CBET_DISCOVER_INDIVIDUAL_ATTRIBUTE_RESPONSE.
Parent topic:General Structures
tsZCL_AttributeDiscoveryExtendedResponse
This structure contains details of an attribute reported in a ‘discover attributes extended’ response. It is contained in a ZCL event of type E_ZCL_CBET_DISCOVER_INDIVIDUAL_ATTRIBUTE_EXTENDED_RESPONSE.
typedef struct
{
bool_t bDiscoveryComplete;
uint16 u16AttributeEnum;
teZCL_ZCLAttributeType eAttributeDataType;
uint8 u8AttributeFlags;
}tsZCL_AttributeDiscoveryExtendedResponse;
where:
bDiscoveryComplete
indicates whether this is the final attribute from a ‘discover attributes’ to be reported:TRUE - final attribute
FALSE - not final attribute
u16AttributeEnum
is the identifier of the attribute being reportedeAttributeDataType
indicates the data type of the attribute being reported (see Section 7.1.3)u8AttributeFlags
is a 5-bit bitmap indicating the accessibility of the reported attribute (for details of the access types, refer to Section 2.3.1) - a bit is set to ‘1’ if the corresponding access type is supported, as follows:
Bit |
Access Type |
---|---|
0 |
Read |
1 |
Write |
2 |
Reportable |
3 |
Scene |
4 |
Global |
5-7 |
Reserved |
The above structure is contained in the tsZCL_CallBackEvent
event structure, detailed in Section 6.2, when the field eEventType
is set to E_ZCL_CBET_DISCOVER_INDIVIDUAL_ATTRIBUTE_EXTENDED_RESPONSE.
Parent topic:General Structures
tsZCL_ReportAttributeMirror
This structure contains information relating to a report attribute command:
typedef struct
{
uint8 u8DestinationEndPoint;
uint16 u16ClusterId;
uint64 u64RemoteIeeeAddress;
teZCL_ReportAttributeStatus eStatus;
}tsZCL_ReportAttributeMirror;
where:
u8DestinationEndPoint
is the number of target endpoint for the attribute report (this is the endpoint on which the mirror for the device resides)u16ClusterId
is the ID of the cluster for which information is to be mirroredu64RemoteIeeeAddress
is the IEEE/MAC address of the target device for the attribute report (which contains the mirror for the device)eStatus
indicates the status of the attribute report (see Section 7.1.5)
Parent topic:General Structures
tsZCL_OctetString
This structure contains information on a ZCL octet (byte) string. This string is of the format:
|Octet Count, N
(1 octet)
|Data
(N octets)
|
which contains N+1 octets, where the leading octet indicates the number of octets (N) of data in the remainder of the string (valid values are from 0x00 to 0xFE).
The tsZCL_OctetString
structure incorporates this information as follows:
typedef struct
{
uint8 u8MaxLength;
uint8 u8Length;
uint8 *pu8Data;
} tsZCL_OctetString;
Where:
u8MaxLength
is the maximum number of data octets in an octet stringu8Length
is the actual number of data octets (N) in this octet stringpu8Data
is a pointer to the first data octet of this string
Note that there is also a tsZCL_LongOctetString
structure in which the octet count (N) is represented by two octets, thus allowing double the number of data octets.
Parent topic:General Structures
tsZCL_CharacterString
This structure contains information on a ZCL character string. This string is of the format:
Character Data Length, L |
Character Data |
---|---|
(1 byte) |
(L bytes) |
which contains L+1 bytes, where the leading byte indicates the number of bytes (L) of character data in the remainder of the string (valid values are from 0x00 to 0xFE). This value represents the number of characters in the string only if the character set used encodes each character using one byte (this is the case for ISO 646 ASCII but not in all character sets, for example, UTF8).
The tsZCL_CharacterString
structure incorporates this information as follows:
typedef struct
{
uint8 u8MaxLength;
uint8 u8Length;
uint8 *pu8Data;
} tsZCL_CharacterString;
where:
u8MaxLength
is the maximum number of character data bytesu8Length
is the actual number of character data bytes (L) in this stringpu8Data
is a pointer to the first character data byte of this string
The string is not null-terminated and may therefore contain null characters mid-string.
Note that there is also a sZCL_LongCharacterString
structure in which the character data length (L) is represented by two bytes, thus allowing double the number of characters.
Parent topic:General Structures
tsZCL_ClusterCustomMessage
This structure contains a cluster custom message:
typedef struct {
uint16 u16ClusterId;
void *pvCustomData;
} tsZCL_ClusterCustomMessage;
Where:
u16ClusterId
is the Cluster ID.pvCustomData
is a pointer to the start of the data contained in the message.
Parent topic:General Structures
tsZCL_ClusterInstance
This structure contains information about an instance of a cluster on a device:
struct tsZCL_ClusterInstance
{
bool_t bIsServer;
tsZCL_ClusterDefinition *psClusterDefinition;
void *pvEndPointSharedStructPtr;
uint8 *pu8AttributeControlBits;
void *pvEndPointCustomStructPtr;
tfpZCL_ZCLCustomcallCallBackFunction
pCustomcallCallBackFunction;
};
where:
bIsServer
indicates whether the cluster instance is a server or client:TRUE - server
FALSE - client
psClusterDefinition
is a pointer to the cluster definition structure - see Section 6.1.2pvEndPointSharedStructPtr
is a pointer to the shared device structure that contains the cluster’s attributespu8AttributeControlBits
is a pointer to an array of bitmaps, one for each attribute in the relevant cluster - for internal cluster definition use only, array should be initialized to 0pvEndPointCustomStructPtr
is a pointer to any custom data (only relevant to a user-defined cluster)pCustomcallCallBackFunction
is a pointer to a custom callback function (only relevant to a user-defined cluster)
Parent topic:General Structures
tsZCL_CommandDiscoveryIndividualResponse
This structure contains information about an individual command reported in a Command Discovery response (see Section 2.9).
typedef struct
{
uint8 u8CommandEnum;
uint8 u8CommandIndex;
} tsZCL_CommandDiscoveryIndividualResponse;
where:
u8CommandEnum
is the Command ID of the reported commandu8CommandIndex
is the index of the reported command in the response payload
The above structure is contained in the tsZCL_CallBackEvent
event structure, detailed in Section 6.2, when the field eEventType
is set to E_ZCL_CBET_DISCOVER_INDIVIDUAL_COMMAND_RECEIVED_RESPONSE or E_ZCL_CBET_DISCOVER_INDIVIDUAL_COMMAND_GENERATED_RESPONSE.
Parent topic:General Structures
tsZCL_CommandDiscoveryResponse
This structure contains information about a Command Discovery response (see Section 2.9).
typedef struct
{
bool_t bDiscoveryComplete;
uint8 u8NumberOfCommands;
} tsZCL_CommandDiscoveryResponse;
Where:
bDiscoveryComplete
is a Boolean flag which indicates whether the Command Discovery is complete, i.e. whether there are any commands remaining to be discovered:TRUE - all commands have been discovered
FALSE - there are further commands to be discovered
u8NumberOfCommands
is the number of discovered commands reported in the response (the individual commands are reported in a structure of the typetsZCL_CommandDiscoveryIndividualResponse
- see Section 6.1.17)
The above structure is contained in the tsZCL_CallBackEvent
event structure, detailed in Section 6.2, when the field eEventType
is set to E_ZCL_CBET_DISCOVER_COMMAND_RECEIVED_RESPONSE or E_ZCL_CBET_DISCOVER_COMMAND_GENERATED_RESPONSE.
Parent topic:General Structures
tsZCL_CommandDefinition
This structure contains the details of a command which is supported by the cluster (and can be reported in Command Discovery).
struct tsZCL_CommandDefinition
{
uint8 u8CommandEnum;
uint8 u8CommandFlags;
};
Where:
u8CommandEnum
is the Command ID within the clusteru8CommandFlags
is a bitmap containing a set of control flags, as follows:
Bits |
Enumeration |
Description |
---|---|---|
0 |
E_ZCL_CF_RX |
Command is generated by the client and received by the server |
1 |
E_ZCL_CF_TX |
Command is generated by the server and received by the client |
2 |
- |
Reserved |
3 |
E_ZCL_CF_MS |
Command is manufacturer-specific |
4 - 7 |
- |
Reserved |
Parent topic:General Structures
tsZCL_SceneExtensionTable
This structure contains a Scenes Extension table.
typedef struct
{
tfpZCL_SceneEventHandler pSceneEventHandler;
uint16 u16NumberOfAttributes;
uint16 au16Attributes[];
} tsZCL_SceneExtensionTable;
Where:
pSceneEventHandler
is a pointer a Scenes event handler functionu16NumberOfAttributes
is the number of attributes in the Scene extensionau16Attributes
is an array of the attribute IDs of the attributes in the Scene extension
Parent topic:General Structures
tsZCL_WriteAttributeRecord
The is structure contains the details for a ‘write attribute’ operation.
typedef struct
{
teZCL_ZCLAttributeType eAttributeDataType;
uint16 u16AttributeEnum;
uint8 *pu8AttributeData;
}tsZCL_WriteAttributeRecord;
Where:
eAttributeDataType
is an enumeration indicating the attribute data type (for the enumerations, refer to Section 7.1.3).u16AttributeEnum
is an enumeration for the attribute identifier (for the relevant ‘Attribute ID’ enumerations, refer to the ‘Enumerations’ section of each cluster-specific chapter).pu8AttributeData
is a pointer to the attribute data to be written.
Parent topic:General Structures
Parent topic:ZCL Structures
Event Structure (tsZCL_CallBackEvent)
A ZCL event must be wrapped in the following tsZCL_CallBackEvent
structure before being passed into the function vZCL_EventHandler():
typedef struct
{
teZCL_CallBackEventType eEventType;
uint8 u8TransactionSequenceNumber;
uint8 u8EndPoint;
teZCL_Status eZCL_Status;
union {
tsZCL_IndividualAttributesResponse sIndividualAttributeResponse;
tsZCL_DefaultResponse sDefaultResponse;
tsZCL_TimerMessage sTimerMessage;
tsZCL_ClusterCustomMessage sClusterCustomMessage;
tsZCL_AttributeReportingConfigurationRecord
sAttributeReportingConfigurationRecord;
tsZCL_AttributeReportingConfigurationResponse
sAttributeReportingConfigurationResponse;
tsZCL_AttributeDiscoveryResponse sAttributeDiscoveryResponse;
tsZCL_AttributeStatusRecord sReportingConfigurationResponse;
tsZCL_ReportAttributeMirror sReportAttributeMirror;
uint32 u32TimerPeriodMs;
tsZCL_CommandDiscoveryIndividualResponse
sCommandsReceivedDiscoveryIndividualResponse;
tsZCL_CommandDiscoveryResponse sCommandsReceivedDiscoveryResponse;
tsZCL_CommandDiscoveryIndividualResponse
sCommandsGeneratedDiscoveryIndividualResponse;
tsZCL_CommandDiscoveryResponse sCommandsGeneratedDiscoveryResponse;
tsZCL_AttributeDiscoveryExtendedResponse
sAttributeDiscoveryExtenedResponse;
}uMessage ;
ZPS_tsAfEvent *pZPSevent;
tsZCL_ClusterInstance *psClusterInstance;
} tsZCL_CallBackEvent;
where
eEventType
: specifies the type of event generated - see Section 7.3.u8TransactionSequenceNumber
is the Transaction Sequence Number (TSN) of the incoming ZCL message (if any) which triggered the ZCL event.u8EndPoint
is the endpoint on which the ZCL message (if any) was received.eZCL_Status
is the status of the operation that the event reports - see Section 7.2uMessage
is a union containing information that is only valid for specific events:s``I``ndividualAttributeResponse
contains the response to a ‘read attributes’ or ‘write attributes’ request - see Section 6.1.8.sDefaultResponse
contains the response to a request (other than a read request) - see Section 6.1.9.sTimerMessage
contains the details of a timer event - this feature is included for future use.sClusterCustomMessage
contains details of a cluster custom command - see Section 6.1.15sAttributeReportingConfigurationRecord
contains the attribute reporting configuration data from the ‘configure reporting’ request for an attribute - see Section 6.1.5.sAttributeReportingConfigurationResponse
is reserved for future use.sAttributeDiscoveryResponse
contains the details of an attribute reported in a ‘discover attributes’ response - see Section 6.1.10.sReportingConfigurationResponse
is reserved for future use.sReportAttributeMirror
contains information on the device from which a ZCL ‘report attribute’ command has been received.u32TimerPeriodMs
contains the timed period of the millisecond timer which is enabled by the application when the event E_ZCL_CBET_ENABLE_MS_TIMER occurs.s``CommandsReceivedDiscoveryIndividualResponse
contains information about an individual command (that can be received) reported in a Command Discovery response - see Section 6.1.17.sCommandsReceivedDiscoveryResponse
contains information about a Command Discovery response which reports commands that can be received - see Section 6.1.18.sCommandsGeneratedDiscoveryIndividualResponse
contains information about an individual command (that can be generated) reported in a Command Discovery response - see Section 6.1.17.sCommandsGeneratedDiscoveryResponse
contains information about a Command Discovery response which reports commands that can be generated - see Section 6.1.18.sAttributeDiscoveryExtenedResponse
contains information from a Discover Attributes Extended response - see Section 6.1.11.
The remaining fields are common to more than one event type but are not valid for all events:
pZPSevent
is a pointer to the stack event (if any) that caused the ZCL event.psClusterInstance
is a pointer to the cluster instance structure that holds the information relating to the cluster being accessed.
Parent topic:ZCL Structures