RAW/POR image switch
In current delivered SDK package, most demos generate RAW images. To enhance customer OOBE experience, the following RT1186 SDK CM33 project/targets generate POR image, which means that they can POR run after you debug/download it in IDE.
IAR/GCC/MDK, hello_world_demo_cm33 flexspi_nor_debug/release, flexspi_nor_hyperram_debug/release
IAR/GCC/MDK, multicore_hello_world_cm33 flexspi_nor_debug/release, flexspi_nor_hyperram_debug/release
MCUX CM33 image are all POR images except the
multicore_trigger
demo.
Note:
These POR images are not signed, just for develop convenience, not recommended for product usage.
It is highly recommended to use SPT for image download.
For the SDK CM33 IAR/MDK/ARMGCC project, flexspi_nor
targets, as well as for MCUX project, debug/release targets. It is easy to switch RAW/POR image, via the project macro XIP_BOOT_HEADER_ENABLE
setting. Table 1describes the rules.
XIP_BOOT_HEADER_ENABLE setting |
Image type |
---|---|
1 |
POR |
0 |
RAW |
For IAR/ARMGCC, change the macro
XIP_BOOT_HEADER_ENABLE
in the compiler setting.For MDK, change the macro
XIP_BOOT_HEADER_ENABLE
in compiler and link setting simultaneously.
For detailed settings, see the following sections.
IAR settings for image type switch
Parent topic:RAW/POR image switch
ARMGCC settings for image type switch
Parent topic:RAW/POR image switch
MDK setting for image type switch
Parent topic:RAW/POR image switch
MCUxpresso settings for image type switch
Parent topic:RAW/POR image switch
Parent topic:Bootable image generation