Bootable image generation

RT1180 can only boot from CM33. For CM33 application image to boot, a sophisticated boot header structure is needed. To ease the customer from complex settings, the Secure Provisioning Tool is provided. Among other rich features, it provides an easy way to use GUI for customer to generate bootable image from raw application image. In addition, in order for users to run the CM7 image conveniently, SDK provides the multicore_trigger demo for users to kick off CM7 image, combined with the SPT tool, we can run CM7 image by from POR.

In this section, two kinds of images are defined

Terminology

Description

RAW image

Demo image without boot header

POR image

Demo image with boot header

Most examples that provided in the SDK package create RAW images from project settings. Only some OOBE examples can create POR image. POR image can provide good out-of-box experience, but the cost is losing some flexibility. While RAW images, with the usage of Secure Provisioning Tool, have the most widely usage like image signning, multiple image combination, and so on. For demos that by default generate a POR boot image, see RAW/POR image switch.

Use SPT tool to boot cm33 image

Run the Secure Provisioning Tool, and the following GUI shows.

Select the following items:

  1. Toolchain generated images

    All SDK generated images are supported no matter they boot from TCM, FlexSPI Nor, or HyperRAM.

    Toolchain

    Suffix

    ARMGCC

    .elf

    IAR

    .out

    MDK

    .out/.hex

    MCUX

    .axf

    Note:

    • Use the RAW image for CM33. Some SDK project targets are POR image by default, it must to be switched to RAW image for SPT usage. For more information, see RAW/POR image switch.

    • It is recommended to use elf/out files, thus SPT can parse the Start address automatically.

  2. XMCD file

    This is on-board HyperRAM initialization file. For the RT1186 FRDM board, select boards/frdmimxrt1186/xmcd/hyperram_xmc_auto_detect.bin.

    Note:

    • If the application image uses hyperram (target hyperram_debug/release, flexspi_hyperram_debug/release, hyperram_txt_debug/release), the XMCD is necessary.

    • hyperram_xmc_auto_detect.bin is board specific.

  3. (Optional) ELE firmware

    This is needed for certain application images which need special ELE FW service. For most SDK demos, simply leave it empty.

After the selection, click Build Image to generate the bootable image (POR image).

Now switch to the Write Image tab. All information is automatically generated from the previous page. Connect both USB OTG1 port (J63) and MCU-Link port (J23) to the computer and power up the board (or reset via SW2). Make sure that the FRDM board boot configuration switch J60[1..3] are on 100 SDP mode and click Write Image.

Change the J60[1..3] to QSPI boot mode 001 and reset the board, and then you can observe that the image is running from POR boot.

Parent topic:Bootable image generation

Use SPT tool and multicore_trigger image to kick off cm7 binary image

This section introduces how to create a CM7 POR boot image with the aid of a CM33 kicker application. The CM33 kicker application is located in demo_apps/multicore_trigger.

For a secure provisioning tool to generate such a bootable CM7 image, specify the CM33 multicore_trigger image in Source executable image. The CM7 application image to be kicked off must be specified with additional images.

CM7 XIP image runs from external FLASH, and multicore_trigger CM33 image runs from internal RAM

Perform the following steps:

  1. Prepare the multicore_trigger_demo_cm33 ram image (debug or release targets) and specify it in Source executable image.

  2. Specify the XMCD file if necessary, refer to Use SPT tool to boot cm33 image.

  3. Use Additional images to specify CM7 application image running from flash memory. See Table 1 for how to fill in the necessary information for this additional image.

    Parameter

    Value

    Explanation

    Image offset

    0x007FF000

    The offset in bytes from the beginning of the current container header to beginning of the image. In our case, the CM7 image is flashed to 0x0480_0000. The container header is put to 0x0400_1000 and the yield offset = 0x7F_F000

    Load address

    0x04800000

    The destintion address of the CM7 image. ROM copies the image to load address, if it is not within flash address space. In our case, copy does not happen

    Entry point

    0x04800000

    The start address of CM7 image vector table from the CM7 core address space

    Core ID

    cortex-m7

    Specify the core ID

    Image type

    Executable

    Specify the image type

    Encrypted

    No

    Specify the encryption

  4. (Optional) ELE firmware.

    It is required for certain application images which need special ELE FW service. For most SDK demos, leaves it empty.

  5. Use Build image to build the combined bootable image. J60[1..3] needs to be set to 100 to let the SOC in serial download mode here.

  6. Use Write image to flash the image.

After a successful write, change the J60[1..3] to QSPI boot mode 001 and reset the board. You can observe that the image is running from POR boot.

Parent topic:Use SPT tool and multicore_trigger image to kick off cm7 binary image

CM7 binary image runs from internal TCM, and multicore_trigger CM33 image runs from external FLASH

Note: Be very careful that this scenario requires fuse manipulation, which is not revertible.

  1. Prepare the multicore_trigger_demo_cm33 flash target image (flexspi_nor_debug or flexspi_nor_release) and specify it in Source executable image.

  2. Use Additional images to specify CM7 application image running from ITCM memory. See Table 1 for how to fill in necessary information for this additional image.

    Parameter

    Value

    Explanation

    Image offset

    0xFF000

    The offset in bytes from the beginning of the current container header to beginning of the image. In our case, the CM7 TCM image is flashed to 0x0410_0000. The container header is put to 0x0400_1000 and the yield offset = 0xF_F000

    Load address

    0x303C0000

    The secured alias of CM7 ITCM in CM33/ROM memory space. ROM will copy image to this address

    Entry point

    0x0

    The start address of vector table from CM7 core address space

    Core ID

    cortex-m7

    Specify the core ID

    Image type

    Executable

    SPecify the image type

    Encrypted

    No

    Specify the encryption

  3. For ROM to successful copy image from flash to CM7 TCM. CM7 TCM ECC should be pre-configured. To archive this, a Fuse need to be set. Click OTP configuration, set POR_PRELOAD_CM7_TCM_ECC and RELEASE_M7_RST_STAT fuses in BOOT_CFG7 to 1.

    Note: Be very careful that any setting on OTP cannot be reverted once set. There is possibility that the chip get bricked if you are fusing the wrong fuse word. Only do this if you really need to try this boot scenario.

  4. (Optional) ELE firmware.

    It is needed for a certain application image which needs a special ELE FW service. For most SDK demos, simply leave it empty.

After a successful write, change the J60[1..3] to QSPI boot mode 001 and reset the board. You can observe that the image is running from the POR boot.

Note:

  1. The new image constructed under Build images is still not a complete image, and the Memory Configuration Block is missing. When writing image, SPT downloads the contents of the Memory Configuration Block to FLASH.

  2. When CM33 + CM7 image runs with the following target combination, it is required to set CM33_SET_TRDC to 1U in multicore_trigger demo, also requires to set CM33_SET_TRDC to 1U in CM7 demo if it exists.

    - CM33 flexspi + CM7 flexspi, flexspi means flexspi_nor_debug/release, flexspi_nor_sdram_debug/release, flexspi_nor_hyperram_debug/release
    - CM33 HYPERRAM + CM7 HYPERRAM, HYPERRAM means hyperram_txt_debug/release.
    
  3. Only those cm7 projects whose linkages are similar with hello_world_demo_cm7, support POR run via multicore_trigger_cm33.

Parent topic:Use SPT tool and multicore_trigger image to kick off cm7 binary image

Parent topic:Bootable image generation

RAW/POR image switch

In current delivered SDK package, most demos generate RAW images. To enhance customer OOBE experience, the following RT1186 SDK CM33 project/targets generate POR image, which means that they can POR run after you debug/download it in IDE.

  • IAR/GCC/MDK, hello_world_demo_cm33 flexspi_nor_debug/release, flexspi_nor_hyperram_debug/release

  • IAR/GCC/MDK, multicore_hello_world_cm33 flexspi_nor_debug/release, flexspi_nor_hyperram_debug/release

  • MCUX CM33 image are all POR images except the multicore_trigger demo.

Note:

  • These POR images are not signed, just for develop convenience, not recommended for product usage.

  • It is highly recommended to use SPT for image download.

For the SDK CM33 IAR/MDK/ARMGCC project, flexspi_nor targets, as well as for MCUX project, debug/release targets. It is easy to switch RAW/POR image, via the project macro XIP_BOOT_HEADER_ENABLE setting. Table 1describes the rules.

XIP_BOOT_HEADER_ENABLE setting

Image type

1

POR

0

RAW

  • For IAR/ARMGCC, change the macro XIP_BOOT_HEADER_ENABLE in the compiler setting.

  • For MDK, change the macro XIP_BOOT_HEADER_ENABLE in compiler and link setting simultaneously.

For detailed settings, see the following sections.

IAR settings for image type switch

Parent topic:RAW/POR image switch

ARMGCC settings for image type switch

Parent topic:RAW/POR image switch

MDK setting for image type switch

Parent topic:RAW/POR image switch

MCUxpresso settings for image type switch

Parent topic:RAW/POR image switch

Parent topic:Bootable image generation

Use Secure Provisiong Tool to erase flash

In worst cases a debugger cannot successfully connect to the board. A major reason for this is there are POR boot image inside the on board flash memory which causes the whole system in a trouble state. Secure Provisioning Tool provide a reliable way to erase the flash in this worst case. To achieve this

  1. Set J60[1..3] to 100.

  2. Connect the board to your PC from both J23 (Debugging) and J63 (USB OTG 1), then power up the board.

  3. Start Secure Provisioning Tool, select Tool > Flash Programmer or Ctrl + R.

  4. Click Yes to prompt up questions, wait memory initialization finish.

  5. Click Erase all button and wait a minute for the erase process to finish.

  6. After Success: Erase whole memory shows up, the board should have restored to a good state to work in various mode.

Parent topic:Bootable image generation