eCLD_IASWDUpdate
teZCL_Status eCLD_IASWDUpdate(
uint8 u8SourceEndPoint);
Description
This function can be used on an IAS WD cluster server to update the timing requirements of the Warning Device. The function should be called by the application at a rate of once every 100 ms.
Parameters
u8SourceEndPointId: Number of the endpoint on which the IAS WD cluster resides
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Functions