Functions
The following IAS WD cluster functions are provided in the NXP implementation of the ZCL:
eCLD_IASWDCreateIASWD
teZCL_Status eCLD_IASWDCreateIASWD(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
void *pvEndPointSharedStructPtr,
uint8 *pu8AttributeControlBits,
tsCLD_IASWDCustomDataStructure
*psCustomDataStructure);
Description
This function creates an instance of the IAS WD cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates an IAS WD cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.
Note: This function must not be called for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.
When used, this function must be called after the stack has been started and after the ZCL has been initialized.
Parameters
psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initializing individual structure fields.
bIsServer: Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the IAS WD cluster. This parameter can refer to a pre-filled structure called
sCLD_``IASWDwhich is provided in the IASWarningDevice.h file.pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_IASWDwhich defines the attributes of IAS WD cluster. The function initializes the attributes with default values.pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster.
psCustomDataStructure: Pointer to a structure containing the storage for internal functions of the cluster (see Section 39.6.1)
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_IASWDUpdate
teZCL_Status eCLD_IASWDUpdate(
uint8 u8SourceEndPoint);
Description
This function can be used on an IAS WD cluster server to update the timing requirements of the Warning Device. The function should be called by the application at a rate of once every 100 ms.
Parameters
u8SourceEndPointId: Number of the endpoint on which the IAS WD cluster resides
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Functions
eCLD_IASWDUpdateMaxDuration
teZCL_Status eCLD_IASWDUpdateMaxDuration(
uint8 u8SourceEndPointId,
uint16 u16MaxDuration);
Description
This function can be used on an IAS WD cluster server to set the value of the u16MaxDuration attribute, which represents the maximum duration, in seconds, for which the alarm can be continuously active.
The set value is the maximum duration, in seconds, for which the alarm can be active following a received Start Warning request.
Parameters
u8SourceEndPointId: Number of the endpoint on which the IAS WD cluster resides
u16MaxDuration: Value to which attribute will be set, in the range 0 to 65534
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Functions
eCLD_IASWDStartWarningReqSend
teZCL_Status eCLD_IASWDStartWarningReqSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_IASWD_StartWarningReqPayload *psPayload);
Description
This function can be used on IAS WD cluster client to send a Start Warning command to the IAS WD server on a Warning Device.
The receiving IAS WD server activates the alarm on the Warning Device for a specified duration.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the command and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload: Pointer to a structure containing the payload for the command (see Section 39.6.2)
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
eCLD_IASWDSquawkReqSend
teZCL_Status eCLD_IASWDSquawkReqSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber,
tsCLD_IASWD_SquawkReqPayload *psPayload);
Description
This function can be used on IAS WD cluster client to send a Squawk command to the IAS WD server on a Warning Device.
The receiving IAS WD server will briefly activate the alarm on the Warning Device to emit a ‘squawk’ - depending on the device, this could be a visible and/or audible emission. The parameters of the squawk are specified in the command payload.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the command and to identify the instance of the shared structure holding the required attribute values
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request
psPayload: Pointer to a structure containing the payload for the command (see Section 39.6.2)
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions
Parent topic:IAS Warning Device Cluster