eCLD_IASWDUpdateMaxDuration
teZCL_Status eCLD_IASWDUpdateMaxDuration(
uint8 u8SourceEndPointId,
uint16 u16MaxDuration);
Description
This function can be used on an IAS WD cluster server to set the value of the u16MaxDuration attribute, which represents the maximum duration, in seconds, for which the alarm can be continuously active.
The set value is the maximum duration, in seconds, for which the alarm can be active following a received Start Warning request.
Parameters
u8SourceEndPointId: Number of the endpoint on which the IAS WD cluster resides
u16MaxDuration: Value to which attribute will be set, in the range 0 to 65534
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Functions