MCUXpresso SDK Documentation

adc_interrupt

adc_interrupt#

Overview#

The qn_adc_interrupt example shows how to use QN ADC driver in the simplest way.

In this example, user should provide a voltage(from 0v to 2.7v) signal on the PA08 pin as the ADC’s sample input. When user type in any key from the keyboard, the software trigger API is called to start the conversion. Then it polls the conversion completed flag till the conversion is completed. Then read the conversion result value and print it to debug console.

Running the demo#

When the example runs successfully, following information can be seen on the OpenSDA terminal:

ADC interrupt example. Configuration Done. Press any key to get demo channel’s ADC value … Original: 0x401e9081 Ch: 8 Result: 1800.470825(mv) Original: 0x401e8eb5 Ch: 8 Result: 1800.265625(mv) Original: 0x401e8e85 Ch: 8 Result: 1800.244141(mv) Original: 0x401e8e21 Ch: 8 Result: 1800.199707(mv)

…