MCUXpresso SDK Documentation

SDK Builder#

Download customized MCUXpresso SDK packages using the online SDK Builder tool.

Overview#

The SDK Builder (https://mcuxpresso.nxp.com/) provides a web-based interface to create customized SDK packages with:

  • Board-specific configurations

  • Selected middleware components

  • Chosen toolchain support

  • Example applications

  • Documentation

This method is ideal for:

  • Offline development environments

  • Classic IDE workflows (IAR, Keil, MCUXpresso IDE)

  • Controlled SDK versions

  • Environments with limited internet access

Accessing SDK Builder#

Step 1: Navigate to SDK Builder#

Visit: https://mcuxpresso.nxp.com/

Step 2: Select Your Board#

  1. Click Select Development Board

  2. Browse or search for your board (e.g., “FRDM-MCXW23”)

  3. Click on your board to select it

Alternatively, select by processor:

  1. Click Select a Processor

  2. Choose your MCU family and specific part number

Step 3: Review Board Information#

The SDK Builder displays:

  • Board overview and features

  • Supported peripherals

  • Available middleware

  • Documentation links

Configuring Your SDK Package#

Toolchain Selection#

Select the toolchains you plan to use:

  • ☑ MCUXpresso IDE - NXP’s Eclipse-based IDE

  • ☑ IAR Embedded Workbench - Professional development environment

  • ☑ Keil MDK - ARM ecosystem integration

  • ☑ ARMGCC / VSCODE - Open-source toolchain

Recommendation: Select toolchain you might use, the ARMGCC / VSCODE is exclusive option comparing to others.

Operating System Selection#

Choose RTOS support:

  • ☑ Bare Metal - No RTOS, direct hardware access

  • ☑ FreeRTOS - Popular open-source RTOS

  • ☐ Zephyr - (Use GitHub installation for Zephyr)

Recommendation: Include FreeRTOS even for bare-metal projects. Examples are valuable learning resources.

Middleware Components#

Select middleware based on your application needs:

Connectivity:

  • ☑ USB Stack - USB device/host/OTG support

  • ☑ lwIP - Lightweight TCP/IP stack

  • ☑ FatFs - FAT file system

  • ☐ Ethernet - If your board has Ethernet

Wireless:

  • ☑ Bluetooth LE - For BLE-enabled MCUs

  • ☑ IEEE 802.15.4 - For Thread/Zigbee applications

  • ☐ Wi-Fi - If using Wi-Fi modules

Graphics:

  • ☐ emWin - GUI library (if using displays)

  • ☐ LVGL - Open-source GUI library

Security:

  • ☑ mbedTLS - Cryptographic library

  • ☐ Secure Subsystem - For secure boot/TrustZone

Audio/Voice:

  • ☐ Voice Seeker - Voice recognition

  • ☐ Audio Processing - DSP libraries

Machine Learning:

  • ☐ eIQ - ML inference engines

  • ☐ TensorFlow Lite Micro

Tip: Start with minimal selection. You can always download additional components later.

Example Applications#

Choose example categories:

  • ☑ demo_apps - Full-featured demonstrations

  • ☑ driver_examples - Peripheral driver examples

  • ☑ hello_world - Basic getting started example

  • ☐ rtos_examples - RTOS usage examples

  • ☐ usb_examples - USB stack examples

  • ☐ middleware_examples - Middleware demonstrations

Recommendation: Include demo_apps and driver_examples for comprehensive learning resources.

Downloading the SDK#

Step 1: Review Configuration#

Click Review Configuration to see your selections:

  • Total package size estimate

  • Included components list

  • Toolchain support

Step 2: Download#

  1. Click Download SDK

  2. Accept the license agreement

  3. Optionally provide email for notifications

  4. Click Download

The SDK downloads as a ZIP archive (typically 500 MB - 2 GB depending on selections).

Step 3: Save the Archive#

Save the ZIP file to a known location:

  • C:\MCUXpresso\SDKs\ (Windows)

  • ~/MCUXpresso/SDKs/ (Linux/macOS)

Tip: Include board name and version in filename:

  • SDK_2.15.0_FRDM-MCXW23.zip

Installing the Downloaded SDK#

For MCUXpresso IDE#

  1. Open MCUXpresso IDE

  2. Window → Preferences → MCUXpresso SDK

  3. Click Import SDK Archive

  4. Browse to downloaded ZIP file

  5. Click OK

The SDK is now available for project creation.

For IAR Embedded Workbench#

  1. Extract the ZIP archive to a permanent location

  2. Open IAR EWARM

  3. Navigate to extracted SDK folder

  4. Open example projects from boards/<board>/iar_examples/

For Keil MDK#

  1. Extract the ZIP archive

  2. Install CMSIS Pack from SDK:

    • Navigate to <SDK>/CMSIS_Packs/

    • Double-click the .pack file to install

  3. Open Keil µVision

  4. Create new project using installed pack

For Command Line (ARM GCC)#

  1. Extract the ZIP archive to a permanent location

  2. Navigate to the mcuxsdk folder, build specified example:

west build -b your_board examples/demo_apps/hello_world

Package Structure#

The package structure differs from IAR/MDK/MCUX/CodeWarrior toolchain and ARMGCC/VSCODE toolchain. The former one is the classic SDK package layout, which contains:

SDK_2.x.x_BOARD/
├── boards/                    # Board-specific files
│   └── <board_name>/
│       ├── demo_apps/         # Demo applications
│       ├── driver_examples/   # Driver examples
│       └── project_template/  # Empty project template
├── CMSIS/                     # ARM CMSIS headers
├── components/                # Reusable components
├── devices/                   # Device-specific files
│   └── <device>/
│       ├── drivers/           # Peripheral drivers
│       ├── gcc/               # GCC linker scripts
│       ├── iar/               # IAR linker scripts
│       └── arm/               # Keil linker scripts
├── docs/                      # Documentation
├── middleware/                # Selected middleware
├── rtos/                      # RTOS support
└── tools/                     # Utilities

The latter one is the repository-layout SDK package, which is organized as:

SDK_2.x.x_BOARD/
├── manifests
│   ├── boards
│   │   ├── custom.yml.template
│   │   └── <board_name>.yml
│   ├── scripts
│   │   ├── west_commands
│   │   └── west_commands.yml
│   ├── submanifests
│   │   ├── base.yml
│   │   ├── devices
│   │   └── rtos
│   └── west.yml
└── mcuxsdk
    ├── arch
    │   ├── arm
    │   └── xtensa
    ├── cmake
    │   ├── extension
    │   └── toolchain
    ├── components
    │   ├── adapter.cmake
    │   └── wifi_bt_module
    ├── COPYING-BSD-3
    ├── devices
    │   ├── prj.conf
    │   └── <device_family>
    |      ├── <device_series>
    |      │   ├── <device_part>
    ├── docs
    ├── drivers
    │   ├── acmp
    │   └── ...
    ├── examples
    │   ├── _boards
    |   │   └── <board_name>
    │   ├── _common
    │   ├── demo_apps
    │   └── driver_examples
    ├── firmware
    │   └── edgelock
    ├── middleware
    │   ├── audio_voice
    │   ├── wifi_nxp
    │   └── wireless
    ├── README.md
    ├── rtos
    │   └── freertos
    ├── scripts
    ├── tool_data
    ├── tool.yml
    └── yamllint_config.yml

Updating Your SDK#

SDK Builder releases new versions periodically with:

  • Bug fixes

  • New features

  • Additional board support

  • Updated middleware

Check for Updates#

  1. Visit SDK Builder: https://mcuxpresso.nxp.com/

  2. Select your board

  3. Check version number against your current SDK

Download New Version#

  1. Configure with same selections as before

  2. Download new SDK archive

  3. Extract to new location (keep old version until migration complete)

  4. Update IDE SDK paths or environment variables

Tip: check online documentation for your specific SDK version.

Troubleshooting#

Download Issues#

Download fails or corrupts:

  • Use download manager for large files

  • Verify ZIP integrity after download

  • Try different browser if issues persist

  • Check available disk space (need 2x package size)

Slow download speeds:

  • Download during off-peak hours

  • Use wired connection instead of Wi-Fi

  • Try different network if available

Extraction Issues#

“Cannot extract” or “Corrupted archive”:

  • Verify complete download (check file size)

  • Use 7-Zip or WinRAR instead of built-in tools

  • Re-download if corruption persists

“Path too long” errors (Windows):

  • Extract to shorter path (e.g., C:\SDK\)

  • Enable long path support in Windows 10/11

  • Use 7-Zip which handles long paths better

IDE Integration Issues#

IDE doesn’t recognize SDK:

  • Verify extraction path has no spaces or special characters

  • Check IDE version compatibility in SDK release notes

  • Ensure all archive contents extracted completely

  • Restart IDE after SDK installation

Missing toolchain support:

  • Return to SDK Builder

  • Ensure desired toolchain was selected during configuration

  • Re-download with correct toolchain selection

Example projects won’t build:

  • Verify toolchain installation and version

  • Check environment variables (ARMGCC_DIR, IAR_DIR, etc.)

  • Review example readme for specific requirements

  • Ensure SDK version matches toolchain version requirements

Offline Development#

Classic packages are ideal for offline development:

Setup for Offline Use#

  1. Download complete package with all needed components

  2. Extract to portable location (USB drive, network share)

  3. Install toolchain on development machine

  4. Copy documentation to local drive

  5. Work offline - no internet required after setup

Sharing with Team#

  1. Download SDK once

  2. Extract to network share

  3. Team members point IDE to shared location

  4. Or distribute extracted SDK via internal file sharing

Tip: Include SDK version and configuration in team documentation.

Advanced: Custom SDK Packages#

For enterprise or team use, you can create custom SDK configurations:

Save Configuration#

After configuring SDK Builder:

  1. Note all selections

  2. Document middleware versions

  3. Save configuration for reproducibility

Scripted Downloads#

SDK Builder doesn’t provide API access, but you can:

  1. Document exact configuration steps

  2. Create team guidelines for SDK downloads

  3. Maintain internal SDK repository with approved versions

Additional Resources#

  • SDK Builder: https://mcuxpresso.nxp.com/

  • SDK Documentation: https://docs.mcuxpresso.nxp.com/mcuxsdk/latest/html/index.html

  • NXP Community: https://community.nxp.com/

  • Technical Support: https://www.nxp.com/support