This file contains the general information which can be shared by the examples on this board. The example specific information can be found in readme.md or example_board_readme.md.
General Example Settings#
Hardware requirements#
Micro USB cable
MIMXRT700-EVK board
Personal Computer
Prepare the Demo#
Connect a micro USB cable between the PC host and the USB port on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Project Configuration#
SDK project supports two kinds of configure methods:
Configure by Kconfig, passing configuration flags during build:
west build ....OR configure by modifing the macros in configure file mcux_config.h.
NOTE: The mcux_config.h is generated by Kconfig, if Kconfig is used, don’t modify mcux_config.h directly, because the manual changes will be overwritten by Kconfig. NOTE: When the macros to be modified don’t exist in the mcux_config.h, add them directly in mcux_config.h.
USB example settings#
For eUSB mode, please disable USB_DEVICE_CONFIG_CHARGER_DETECT macro and USB_DEVICE_CONFIG_DETACH_ENABLE. RT700 eUSB does not support DCD feature (device charger detect) and VBUS detection.
For eUSB repeater mode, please populate R417 and R418, and remove R409 and R410. This is default setting on the board. Besides, please use external 5V power adapter to the board to make sure the power supply for eUSB PTN3222 is enough.
For eUSB native mode, please populate R409 and R410, and remove R417 and R418.
Display settings#
This board supports such panels:
TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika (SSD1963)
LCD_PAR_S035 3.5” 480x320 IPS TFT LCD Module (ST7796S)
“RK055HDMIPI4M” MIPI Rectangular Display (RK055AHD091)
“RK055IQH091” MIPI Rectangular panel
“RK055MHD091A0-CTG” MIPI Rectangular Display (RK055MHD091)
“G1120B0MIPI” MIPI Circular Display (RM67162)
RaspberryPi Panel
ZC143AC72MIPI DBI panel (CO5300)
This section describes the general display related settings. Some projects may have special display settings, such as LVGL project. Please refer LVGL project lv_examples_readme.md for the steps.
Board hardware settings#
TFT Proto 5” panel
Connect panel to J4.
Connect JP7 2&3 to use 3.3v interface.
LCD_PAR_S035 panel
Connect panel to J4 pin 1 to pin 28.
Connect JP7 2&3 to use 3.3v interface.
Set SW1 is 0b011 (8 bit 8080).
Remove resistance R60 to use the touch function.
MIPI panels
Connect MIPI panel to J52.
Raspberry panel
Make sure the R75, R76, R79, R80 are connected.
Connect the panel to J8
Connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.
Steps to select the panel#
Please read section Project Configuration to know the configuration methods first.
“RK055MHD091A0-CTG” MIPI rectangular panel (RK055MHD091) is used by default. The panel can be switched by using west build option or modifying mcux_config.h.
Panel |
west build option |
mcux_config.h DEMO_PANEL |
|---|---|---|
TFT Proto 5” CAPACITIVE (SSD1963) |
|
4 |
RK055HDMIPI4M MIPI Rectangular (RK055AHD091) |
|
0 |
MIPI RK055IQH091 panel |
|
1 |
G1120B0MIPI MIPI Circular (RM67162) |
|
3 |
RK055MHD091A0-CTG MIPI Rectanglular (RK055MHD091, default) |
|
2 |
RaspberryPi |
|
5 |
ZC143AC72MIPI MIPI Circular (CO5300) |
|
6 |
LCD_PAR_S035 (ST7796S) |
|
8 |
Panel configuration#
Please read section Project Configuration to know the configuration methods first.
TFT Proto 5” CAPACITIVE Panel (SSD1963)#
Pixel format#
By Kconfig
RGB565(default): Use build parameter
-DCONFIG_DEMO_SSD1963_BUFFER_RGB565=yor omit.RGB888: Use build parameter
-DCONFIG_DEMO_SSD1963_BUFFER_RGB888=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.RGB565(default)
#define DEMO_SSD1963_BUFFER_FORMAT 0RGB888
#define DEMO_SSD1963_BUFFER_FORMAT 1
Driven Peripehral#
By Kconfig
Driven by LCDIF(default): Use build parameter
-DCONFIG_DEMO_PANEL_TFT_PROTO_5_LCDIF=yor omit.Driven by FlexIO: Use build parameter
-DCONFIG_DEMO_PANEL_TFT_PROTO_5_FLEXIO=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.Driven by LCDIF(default)
#define SSD1963_DRIVEN_BY 1Driven by FlexIO
#define SSD1963_DRIVEN_BY 0
Note: When driving panel with FlexIO, only RGB888 pixel format is supported.
RK055HDMIPI4M MIPI Rectangular Panel (RK055AHD091)#
Pixel format#
By Kconfig
RGB565(default): Use build parameter
-DCONFIG_DEMO_RK055AHD091_BUFFER_RGB565=yor omit.XRGB888: Use build parameter
-DCONFIG_DEMO_RK055AHD091_BUFFER_XRGB8888=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.RGB565(default)
#define DEMO_RK055AHD091_USE_XRGB8888 0XRGB888
#define DEMO_RK055AHD091_USE_XRGB8888 1
RK055MHD091A0-CTG MIPI Rectanglular Panel (RK055MHD091)#
Pixel format#
By Kconfig
RGB565(default): Use build parameter
-DCONFIG_DEMO_RK055MHD091_BUFFER_RGB565=yor omit.XRGB888: Use build parameter
-DCONFIG_DEMO_RK055MHD091_BUFFER_XRGB8888=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.RGB565(default)
#define DEMO_RK055MHD091_USE_XRGB8888 0XRGB888
#define DEMO_RK055MHD091_USE_XRGB8888 1
G1120B0MIPI MIPI Circular Panel (RM67162)#
Pixel format#
By Kconfig
RGB565(default): Use build parameter
-DCONFIG_DEMO_RM67162_BUFFER_RGB565=yor omit.RGB888: Use build parameter
-DCONFIG_DEMO_RM67162_BUFFER_RGB888=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.RGB565(default)
#define DEMO_RM67162_BUFFER_FORMAT 0RGB888
#define DEMO_RM67162_BUFFER_FORMAT 1
ZC143AC72MIPI MIPI Circular Panel (CO5300)#
Pixel format#
By Kconfig
RGB565(default): Use build parameter
-DCONFIG_DEMO_CO5300_BUFFER_RGB565=yor omit.RGB888: Use build parameter
-DCONFIG_DEMO_CO5300_BUFFER_RGB888=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.RGB565(default)
#define DEMO_CO5300_BUFFER_FORMAT 0RGB888
#define DEMO_CO5300_BUFFER_FORMAT 1
MIPI RK055IQH091 Rectangular Panel#
Pixel format#
Only RGB565 is supported
RaspberryPi#
Pixel format#
Only RGB565 is supported
LCD_PAR_S035#
Pixel format#
By Kconfig
RGB565(default): Use build parameter
-DCONFIG_DEMO_LCD_PAR_S035_BUFFER_RGB565=yor omit.RGB888: Use build parameter
-DCONFIG_DEMO_LCD_PAR_S035_BUFFER_RGB888=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.RGB565(default)
#define DEMO_LCD_PAR_S035_BUFFER_FORMAT 0RGB888
#define DEMO_LCD_PAR_S035_BUFFER_FORMAT 1
Driven Peripehral#
By Kconfig
Driven by LCDIF(default): Use build parameter
-DCONFIG_DEMO_PANEL_LCD_PAR_S035_LCDIF=yor omit.Driven by FlexIO: Use build parameter
-DCONFIG_DEMO_PANEL_LCD_PAR_S035_FLEXIO=y
Or By modifying
mcux_config.h. If the macros don’t exist, add them directly.Driven by LCDIF(default)
#define ST7796S_DRIVEN_BY 1Driven by FlexIO
#define ST7796S_DRIVEN_BY 0