Getting Started with Package# Overview MCUXpresso SDK board support package folders Example application structure Locating example application source files What is the plain load image? What is the XIP image? What is the SRAM target image? Run a demo application using IAR Build an non-XIP (plain load) example application Run a non-XIP (plain load) example application using CMSIS DAP Run a non-XIP (plain load) example application using J-Link/J-Trace Build an XIP example application Run an XIP example application Run a demo using Keil® MDK/μVision Install CMSIS device pack Build a non-XIP (plain load) example application Run a non-XIP (plain load) example application How to program the non-XIP (plain load) example application to external flash How to program the non-XIP (plain load) example application to external flash using J-Link Build an XIP example application Run an XIP example application Run a demo using Arm® GCC Run a demo using MCUXpresso IDE Select the workspace location Build a non-XIP (plain load) example application Run a non-XIP (plain load) example application How to program the non-XIP (plain load) example bin file to external flash Build an XIP example application Run an XIP example application MCUXpresso Config Tools MCUXpresso IDE New Project Wizard How to determine COM port Default debug interfaces Updating debugger firmware Updating LPCXpresso board firmware How to update SPIFI clock Frequency Updating SPIFI clock frequency in IAR Updating SPIFI clock frequency in Keil® MDK/μVision Updating SPIFI clock frequency in Arm® GCC Updating SPIFI clock frequency in MCUXpresso IDE