MCUXpresso SDK Documentation

MCUXpresso SDK Release Notes#

Development tools#

The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.

  • MCUXpresso IDE, Rev. 25.06.xx

  • IAR Embedded Workbench for Arm, version is 9.70.4

  • Keil MDK, version is 5.43a

  • MCUXpresso for VS Code v26.06

  • GCC Arm Embedded Toolchain 14.2.x

Supported development systems#

This release supports board and devices listed in following table. The board and devices in bold were tested in this release.

Development boards

MCU devices

FRDM-MCXL255

MCXL253VDF, MCXL253VLL, MCXL254VDF,
MCXL254VLL, MCXL255VDF, MCXL255VLL,
MCXL142VDH, MCXL142VLL, MCXL143VDH,
MCXL143VLL, MCXL144VDH, MCXL144VLL

MCUXpresso SDK release package#

The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.

Device support#

The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.

Board support#

The boards folder provides the board-specific demo applications, driver examples, and middleware examples.

Demo application and other examples#

The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.

RTOS#

FreeRTOS#

Real-time operating system for microcontrollers from Amazon

Middleware#

CMSIS DSP Library#

The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.

TF-M#

Trusted Firmware - M Library

PSA Test Suite#

Arm Platform Security Architecture Test Suite

mbedTLS#

mbedtls SSL/TLS library v3.x

NXP PSA CRYPTO DRIVER#

PSA crypto driver for crypto library integration via driver wrappers

NXP SGI PKC#

NXP Secure General Interface Public Key Cryptography middleware for hardware-accelerated asymmetric crypto operations.

MCU Boot#

Open source MCU Bootloader.

Multicore#

Multicore Software Development Kit

FreeMASTER#

FreeMASTER communication driver for 32-bit platforms.

LittleFS#

LittleFS filesystem stack

Release contents#

Provides an overview of the MCUXpresso SDK release package contents and locations.

Deliverable

Location

Boards

INSTALL_DIR/boards

Demo Applications

INSTALL_DIR/boards/<board_name>/demo_apps

Driver Examples

INSTALL_DIR/boards/<board_name>/driver_examples

eIQ examples

INSTALL_DIR/boards/<board_name>/eiq_examples

Board Project Template for MCUXpresso IDE NPW

INSTALL_DIR/boards/<board_name>/project_template

Driver, SoC header files, extension header files and feature header files, utilities

INSTALL_DIR/devices/<device_name>

CMSIS drivers

INSTALL_DIR/devices/<device_name>/cmsis_drivers

Peripheral drivers

INSTALL_DIR/devices/<device_name>/drivers

Toolchain linker files and startup code

INSTALL_DIR/devices/<device_name>/<toolchain_name>

Utilities such as debug console

INSTALL_DIR/devices/<device_name>/utilities

Device Project Template for MCUXpresso IDE NPW

INSTALL_DIR/devices/<device_name>/project_template

CMSIS Arm Cortex-M header files, DSP library source

INSTALL_DIR/CMSIS

Components and board device drivers

INSTALL_DIR/components

RTOS

INSTALL_DIR/rtos

Release Notes, Getting Started Document and other documents

INSTALL_DIR/docs

Tools such as shared cmake files

INSTALL_DIR/tools

Middleware

INSTALL_DIR/middleware

Known Issues#

This section lists the known issues, limitations, and/or workarounds.

Cannot add SDK components into FreeRTOS projects#

It is not possible to add any SDK components into FreeRTOS project using the MCUXpresso IDE New Project wizard.

aon_lpuart_wakeup_mcxl: Continuous print or hang after Deep Power Down 2 wakeup#

When running the aon_lpuart_wakeup_mcxl demo on EBL3.7 silicon, the board may continuously print log messages or hang upon wakeup from Deep Power Down 2 (DPD2) mode.

Compilation error in FREQME driver example — undefined identifier#

A compilation error occurs in the FREQME driver example due to the identifier klNPUTMUX_FreqmeClkIn1ToFreqmeasRef being undefined when clock configuration generated by Clocks Tool is used.

ADVC library outdated#

ADVC library version included in the SDK is outdated and may not be compatible with the latest MCXL25x devices.

VDD_CORE_AON voltages not updated in MCXL power driver, Clock Configuration Tool and SDK clock config files#

The voltage settings in the MCXL power driver, the Clock Configuration Tool and the generated SDK clock configuration files reflect outdated values and are not aligned with the required operating points of AON domain.

TrustZone non-secure example base address is not defined#

The base address for TrustZone non-secure region examples is not defined, thus default west flash command rewrites the secure app.

CM0+ core debug in Keil uVision IDE#

CM0+ core debug using CMSIS-DAP is not supported in Keil uVision IDE.