RAW/POR image switch#
In the current SDK package, most CM33 demos generate POR images by default, while all CM7 demos generate RAW images. To enhance the customer out-of-box experience (OOBE), the following RT1180 SDK CM33 projects/targets generate POR images, meaning they can run in POR mode after you debug or download them in the IDE.
IAR/GCC/MDK, all cm33 examples except the multicore_trigger, target: flexspi_nor_debug/release, flexspi_nor_hyperram_debug/release
MCUXpresso CM33 image are all POR images except the
multicore_triggerdemo.
Note:
These POR images are not signed, just for develop convenience, not recommended for product usage.
It is highly recommended to use SPT for image download.
For the SDK CM33 IAR/MDK/ARMGCC project, flexspi_nor targets, as well as for MCUX project, debug/release targets. It is easy to switch RAW/POR image, via the project macro XIP_BOOT_HEADER_ENABLE setting. Table 1describes the rules.
XIP_BOOT_HEADER_ENABLE setting |
Image type |
|---|---|
1 |
POR |
0 |
RAW |
For IAR/ARMGCC, change the macro
XIP_BOOT_HEADER_ENABLEin the compiler setting.For MDK, change the macro
XIP_BOOT_HEADER_ENABLEin compiler and link setting simultaneously.
For detailed settings, see the following sections.
IAR settings for image type switch#

Parent topic:RAW/POR image switch
ARMGCC settings for image type switch#

Parent topic:RAW/POR image switch
MDK setting for image type switch#


Parent topic:RAW/POR image switch
MCUxpresso settings for image type switch#


Parent topic:RAW/POR image switch
Parent topic:Bootable image generation