Bootable image generation#
RT1180 can only boot from CM33. For CM33 application image to boot, a sophisticated boot header structure is needed. To ease the customer from complex settings, the Secure Provisioning Tool is provided. Among other rich features, it provides an easy way to use GUI for customer to generate bootable image from raw application image. In addition, in order for users to run the CM7 image conveniently, SDK provides the multicore_trigger demo for users to kick off CM7 image, combined with the SPT tool, we can run CM7 image by from POR.
In this section, two kinds of images are defined
Terminology |
Description |
|---|---|
RAW image |
Demo image without boot header |
POR image |
Demo image with boot header |
Most CM33 examples provided in the SDK package generate POR images based on project settings. Only a few examples create RAW images by default. POR images offer a good out-of-the-box experience but reduce flexibility. In contrast, RAW images, when used with the Secure Provisioning Tool, support broader functionality such as image signing, combining multiple images, and more. For demos that generate a POR boot image by default, see RAW/POR image switch.
Use SPT tool to boot cm33 image#
Run the Secure Provisioning Tool, and the following GUI shows.

Select the following items:
Toolchain generated images
All SDK generated images are supported no matter they boot from TCM, FlexSPI Nor, or HyperRAM.
Toolchain
Suffix
ARMGCC
.elf
IAR
.out
MDK
.out/.hex
MCUX
.axf
Note:
Use the RAW image for CM33. For SDK projects whose default target is a POR image, switch to a RAW image for SPT usage. For more information, see RAW/POR image switch.
It is recommended to use elf/out files, thus SPT can parse the Start address automatically.
XMCD file
This is on-board SDRAM/HyperRAM initialization file. For the RT1180 EVK board, select boards/evkmimxrt1180/xmcd/hyperram_xmc_auto_detect.bin.
Note:
If the application image uses
hyperram(target hyperram_debug/release, flexspi_hyperram_debug/release, hyperram_txt_debug/release), the XMCD is necessary.hyperram_xmc_auto_detect.bin is board specific.
(Optional) ELE firmware
This is needed for certain application images which need special ELE FW service. For most SDK demos, simply leave it empty.
After the selection, click Build Image to generate the bootable image (POR image).


Now switch to the Write Image tab. All information is automatically generated from the previous page. Connect both USB OTG1 port (J33) and MCU-Link port (J53) to the computer and power up the board (or reset via SW3). Make sure that the EVK board boot configuration switch SW5[1..4] are on 0001 SDP mode and click Write Image.


Change the SW5[1..4] to QSPI boot mode 0100 and reset the board, and then you can observe that the image is running from POR boot.
Parent topic:Bootable image generation
Use SPT tool and multicore_trigger image to kick off cm7 binary image#
This section introduces how to create a CM7 POR boot image with the aid of a CM33 kicker application. The CM33 kicker application is located in demo_apps/multicore_trigger.
For a secure provisioning tool to generate such a bootable CM7 image, specify the CM33 multicore_trigger image in Source executable image. The CM7 application image to be kicked off must be specified with additional images.

CM7 XIP image runs from external FLASH, and multicore_trigger CM33 image runs from internal RAM#
Perform the following steps:
Prepare the
multicore_trigger_demo_cm33ram image (debugorreleasetargets) and specify it inSource executable image.Specify the XMCD file if necessary, refer to Use SPT tool to boot cm33 image.
Use
Additional imagesto specify CM7 application image running from flash memory. See Table 1 for how to fill in the necessary information for this additional image.
| Parameter | Value | Explanation |
|--------------|--------------|-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------|
| Image offset | `0x007FF000` | The offset in bytes from the beginning of the current container header to beginning of the image. In our case, the CM7 image is flashed to `0x2880_0000`. The container header is put to `0x2800_1000` and the yield offset = `0x7F_F000` |
| Load address | `0x28800000` | The destintion address of the CM7 image. ROM copies the image to load address, if it is not within flash address space. In our case, copy does not happen |
| Entry point | `0x28800000` | The start address of CM7 image vector table from the CM7 core address space |
| Core ID | cortex-m7 | Specify the core ID |
| Image type | Executable | Specify the image type |
| Encrypted | No | Specify the encryption |

(Optional) ELE firmware.
It is required for certain application images which need special ELE FW service. For most SDK demos, leaves it empty.
Use
Build imageto build the combined bootable image.SW5[1..4]needs to be set to0001to let the SOC in serial download mode here.
Use
Write imageto flash the image.

After a successful write, change the SW5[1..4] to QSPI boot mode 0100 and reset the board. You can observe that the image is running from POR boot.
Parent topic:Use SPT tool and multicore_trigger image to kick off cm7 binary image
CM7 binary image runs from internal TCM, and multicore_trigger CM33 image runs from external FLASH#
Note: Be very careful that this scenario requires fuse manipulation, which is not revertible.
Prepare the
multicore_trigger_demo_cm33flash target image (flexspi_nor_debugorflexspi_nor_release) and specify it inSource executable image.Use
Additional imagesto specify CM7 application image running from ITCM memory. See Table 1 for how to fill in necessary information for this additional image.
| Parameter | Value | Explanation |
|--------------|--------------|----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------|
| Image offset | `0xFF000` | The offset in bytes from the beginning of the current container header to beginning of the image. In our case, the CM7 TCM image is flashed to `0x2810_0000`. The container header is put to `0x2800_1000` and the yield offset = `0xF_F000` |
| Load address | `0x303C0000` | The secured alias of CM7 ITCM in CM33/ROM memory space. ROM will copy image to this address |
| Entry point | `0x0` | The start address of vector table from CM7 core address space |
| Core ID | cortex-m7 | Specify the core ID |
| Image type | Executable | SPecify the image type |
| Encrypted | No | Specify the encryption |

For ROM to successful copy image from flash to CM7 TCM. CM7 TCM ECC should be pre-configured. To archive this, a Fuse need to be set. Click OTP configuration, set
POR_PRELOAD_CM7_TCM_ECCandRELEASE_M7_RST_STATfuses inBOOT_CFG7to 1.Note: Be very careful that any setting on OTP cannot be reverted once set. There is possibility that the chip get bricked if you are fusing the wrong fuse word. Only do this if you really need to try this boot scenario.

(Optional) ELE firmware.
It is needed for a certain application image which needs a special ELE FW service. For most SDK demos, simply leave it empty.



After a successful write, change the SW5[1..4] to QSPI boot mode 0100 and reset the board. You can observe that the image is running from the POR boot.
Note:
The new image constructed under Build images is still not a complete image, and the Memory Configuration Block is missing. When writing image, SPT downloads the contents of the Memory Configuration Block to FLASH.
Only cm7 projects with linkages identical or similar to hello_world_demo_cm7 support POR execution via
multicore_trigger_cm33.
Parent topic:Use SPT tool and multicore_trigger image to kick off cm7 binary image
Parent topic:Bootable image generation
RAW/POR image switch#
In the current SDK package, most CM33 demos generate POR images by default, while all CM7 demos generate RAW images. To enhance the customer out-of-box experience (OOBE), the following RT1180 SDK CM33 projects/targets generate POR images, meaning they can run in POR mode after you debug or download them in the IDE.
IAR/GCC/MDK, all cm33 examples except the multicore_trigger, target: flexspi_nor_debug/release, flexspi_nor_hyperram_debug/release
MCUXpresso CM33 image are all POR images except the
multicore_triggerdemo.
Note:
These POR images are not signed, just for develop convenience, not recommended for product usage.
It is highly recommended to use SPT for image download.
For the SDK CM33 IAR/MDK/ARMGCC project, flexspi_nor targets, as well as for MCUX project, debug/release targets. It is easy to switch RAW/POR image, via the project macro XIP_BOOT_HEADER_ENABLE setting. Table 1describes the rules.
XIP_BOOT_HEADER_ENABLE setting |
Image type |
|---|---|
1 |
POR |
0 |
RAW |
For IAR/ARMGCC, change the macro
XIP_BOOT_HEADER_ENABLEin the compiler setting.For MDK, change the macro
XIP_BOOT_HEADER_ENABLEin compiler and link setting simultaneously.
For detailed settings, see the following sections.
IAR settings for image type switch#

Parent topic:RAW/POR image switch
ARMGCC settings for image type switch#

Parent topic:RAW/POR image switch
MDK setting for image type switch#


Parent topic:RAW/POR image switch
MCUxpresso settings for image type switch#


Parent topic:RAW/POR image switch
Parent topic:Bootable image generation
Use Secure Provisiong Tool to erase flash#
In worst cases a debugger cannot successfully connect to the board. A major reason for this is there are POR boot image inside the on board flash memory which causes the whole system in a trouble state. Secure Provisioning Tool provide a reliable way to erase the flash in this worst case. To achieve this
Set SW5[1:4] to
0001.Connect the board to your PC from both
J53(Debugging) andJ33(USB OTG 1), then power up the board.Start
Secure Provisioning Tool, selectTool>Flash ProgrammerorCtrl + R.Click
Yesto prompt up questions, wait memory initialization finish.
Click
Erase allbutton and wait a minute for the erase process to finish.
After
Success: Erase whole memoryshows up, the board should have restored to a good state to work in various mode.
Parent topic:Bootable image generation