MCUXpresso SDK Documentation

Complex Dependency#

MCUXpresso SDK build system provides complex dependencies record and resolve for both sections(examples and components) and sources.

Section Level Dependency#

Kconfig dependency mechanism and tool is used to describe and resolve section level dependency.

Dependency Mechanisms#

Kconfig provides depends on, select and choice dependency mechanisms.

  • depends on

    It defines a dependency for Kconfig symbol. If multiple dependencies are defined, they can be connected with &&, ||, and ! for NOT.

    The Kconfig item won’t be showed if the depends on is not satisfied.

  • select

    It forces a symbol to true which means the depended component is selected anyway no matter its dependency is satisfied or not.

  • choice

    It defines a choice group. The single choice can only be of type bool or tristate. If no type is specified for a choice, its type will be determined by the type of the first choice element in the group or remain unknown if none of the choice elements have a type specified.

Kconfig processor will give detailed warnings about unsatisfied component selection so that you can immediately find it and update.

Practice Recommendation#

  • For software components depending on hardware related dependency items like board, device, device_id, please use depends on. In this way, for any component whose hardware dependencies are not satisfied, it will not be showed so that not bloat the Kconfig GUI.

  • For software components depending on software component, priority to use select. It helps to auto select component dependency.

  • For cycle dependency case like FOO needs to select BAR and BAR needs to select FOO, since Kconfig doesn’t support cycle dependency, so you cannot use mutually select between FOO and BAR. The recommendation is use both select and depends on. For example, FOO select BAR and BAR depends on FOO. In this way, when you tick FOO, then BAR will be automatically selected. When FOO dependency is not satisfied, BAR cannot be showed.

  • If there are any of dependencies, choice can satisfy the need.

Hardware Dependency Items#

Following Harry dependency items are provided for components to depends on:

Dependency Item

Illustration

MCUX_HW_DEVICE_<device>

Device, like MIMXRT1176

MCUX_HW_DEVICE_ID_<device_id>

Device id, like MIMXRT1176xxxxx

MCUX_HW_CORE_<core_name>

Core name, like cm4f

MCUX_HW_CORE_ID_<core_id>

Core id, like cm4

MCUX_HW_BOARD_<board name>

Board name, like evkbmimxrt1170

MCUX_HW_KIT_<kit name>

Kit name, like mimxrt700evk_a8974

MCUX_HW_<fpu type>

fpu type name, like MCUX_HW_FPV4_SP

MCUX_HW_DSP

DSP or no DSP

MCUX_HW_MPU

MPU or no MPU

MCUX_HW_SAU

Secure or nonsecure

All these dependency items shall be defined in device Kconfig.chip.

Source Level Dependency#

Source level dependency is achieved through the CMake extension, like

mcux_add_source(
    SOURCES portable/GCC/ARM_CM0/port.c
    # The following 2 lines mean port.c only supports cm0p core and toolchain armgcc, mcux and mdk
    CORES cm0p
    TOOLCHAINS armgcc mcux mdk
)

Please refer the mcux_add_source/mcux_add_include extension arguments for supported dependency items.