freertos_blinky_s#
Overview#
This document explains the freertos_tzm example. This demo application utilizes TrustZone, so it demonstrates following techniques for TrustZone applications development:
Application separation between secure and non-secure part
TrustZone environment configuration
Exporting secure function to non-secure world
Calling non-secure function from secure world
Configuring IAR, MDK, GCC and MCUX environments for TrustZone based projects
Running the demo#
The Trust Zone-M (TZM) demo creates two unprivileged tasks. One of which calls a secure side function and passes a pointer to a callback function. The secure side function does three things:
It calls the provided callback function. The callback function increments a counter.
It increments a counter and returns the incremented value. After the secure function call finishes, it verifies that both the counters are incremented.
It calls a secure side function to toggle the green LED The second task just calls a secure side function to toggle the blue LED