Requirements for building USB examples#
The TWR-K22F120M Tower System module or FRDM-K64F Freedom platform is used as an example in this document. The process for compiling, downloading, and running examples is similar on all other boards. For a detailed version of the toolchain software, see the MCUXpresso SDK Release Notes (document MCUXSDKRN).
Hardware#
TWR-K22F120M Tower System module and (optional) TWR-SER Tower System module and Elevator
MCUXpresso SDK Boards
J-Link debugger (optional)
USB cables
Parent topic:Requirements for building USB examples
Software#
MCUXpresso SDK release package
IAR Embedded Workbench for Arm Version 8.11.3
Keil µVision5 Integrated Development Environment Version 5.23 , available for Arm Cortex-M4 devices
MCUXpresso IDE v10.1.0
Makefiles support with GCC revision 6-2017-q2-update from Arm Embedded
Parent topic:Requirements for building USB examples
Parent topic:Build the USB examples in MCUXpresso SDK